<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: distro backend for headless device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/distro-backend-for-headless-device/m-p/918663#M138206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gstreamer is part of Multimedia plugins package, you need any multimedia backend to star to work with it, or you can have it in core-image-minimal but you will have to add all the resources they need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jul 2019 14:19:57 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2019-07-29T14:19:57Z</dc:date>
    <item>
      <title>distro backend for headless device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/distro-backend-for-headless-device/m-p/918662#M138205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am planning on building a headless embedded device.&lt;/P&gt;&lt;P&gt;I need gstreamer as I will be doing camera capture but I do have a display.&lt;/P&gt;&lt;P&gt;Normally I would use xwayland or frambuffer as a backend but because this is headless I am wondering if one of the other distro's without a windowing backend might be a better choice? What would be a better selection? Do these more "minimal" distros still support gstreamer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jul 2019 12:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/distro-backend-for-headless-device/m-p/918662#M138205</guid>
      <dc:creator>davidvescovi</dc:creator>
      <dc:date>2019-07-29T12:02:31Z</dc:date>
    </item>
    <item>
      <title>Re: distro backend for headless device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/distro-backend-for-headless-device/m-p/918663#M138206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gstreamer is part of Multimedia plugins package, you need any multimedia backend to star to work with it, or you can have it in core-image-minimal but you will have to add all the resources they need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jul 2019 14:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/distro-backend-for-headless-device/m-p/918663#M138206</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-07-29T14:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: distro backend for headless device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/distro-backend-for-headless-device/m-p/1711004#M211409</link>
      <description>&lt;P&gt;This post doesn't really answer my distro question. Do we really need wayland, weston, etc. to run a headless hardware? Could you please specify the recommended distro configuration?&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 21:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/distro-backend-for-headless-device/m-p/1711004#M211409</guid>
      <dc:creator>moose</dc:creator>
      <dc:date>2023-08-24T21:41:51Z</dc:date>
    </item>
  </channel>
</rss>