<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8 Mini JTAG Interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Mini-JTAG-Interface/m-p/917122#M138031</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;So sorry for late reply. I have confirmed it for you. The power domain of POR_B is VSNVS, the power domian of Jtag IO is DCDC_3V3. External Jtag device output nRST signal to our system, its power domain is different our system.&amp;nbsp;So&amp;nbsp;D1905 and D1906 is for isolation of different power domain, in order to keep the current from flowing back.&lt;/P&gt;&lt;P&gt;Hope this can do help for you.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jun 2019 07:28:48 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2019-06-05T07:28:48Z</dc:date>
    <item>
      <title>i.MX8 Mini JTAG Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Mini-JTAG-Interface/m-p/917121#M138030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking at the schematics for the 8MMINILPD4 base board design JTAG interface to the processor I am curious about the functionality and purpose of diodes D907 and D908.&amp;nbsp; Are these used to to control the nRST and keep the JTAG from overriding POR_B?&amp;nbsp; I have the snapshot from the schematic showing the diodes in question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84048i66C65BC61CE2A470/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 23:05:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Mini-JTAG-Interface/m-p/917121#M138030</guid>
      <dc:creator>shawnnageli</dc:creator>
      <dc:date>2019-05-28T23:05:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Mini JTAG Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Mini-JTAG-Interface/m-p/917122#M138031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;So sorry for late reply. I have confirmed it for you. The power domain of POR_B is VSNVS, the power domian of Jtag IO is DCDC_3V3. External Jtag device output nRST signal to our system, its power domain is different our system.&amp;nbsp;So&amp;nbsp;D1905 and D1906 is for isolation of different power domain, in order to keep the current from flowing back.&lt;/P&gt;&lt;P&gt;Hope this can do help for you.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2019 07:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Mini-JTAG-Interface/m-p/917122#M138031</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-06-05T07:28:48Z</dc:date>
    </item>
  </channel>
</rss>