<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: LPDDR2 Script aid for imx6sl 512 MB dram</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917057#M138027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sujay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can debug it, adding for example gpio toggle in uboot sources.&lt;/P&gt;&lt;P&gt;Check for example function dram_init():&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6slevk/mx6slevk.c?h=imx_v2017.03_4.9.88_2.0.0_ga" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6slevk/mx6slevk.c?h=imx_v2017.03_4.9.88_2.0.0_ga"&gt;mx6slevk.c\mx6slevk\freescale\board - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW what is exact memory size 512 MB or 512 Mb, they are both mentioned in post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Sep 2019 11:03:22 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-09-26T11:03:22Z</dc:date>
    <item>
      <title>LPDDR2 Script aid for imx6sl 512 MB dram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917054#M138024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to run a ddr calibration test for an imx6slevk board with 512 MB lpddr2 Dram.&lt;/P&gt;&lt;P&gt;I found a script aid in this link: &lt;A href="https://community.nxp.com/docs/DOC-94987"&gt;i.MX6SL LPDDR2 Script Aid&lt;/A&gt;&amp;nbsp; however in the comments below, it is mentioned that this scripts is not compatible for 512 Mb Ram.&lt;/P&gt;&lt;P&gt;I tried going through the reference manual and looked at each of the registers mentioned in the .inc file but none of them mention the size.&lt;/P&gt;&lt;P&gt;Can anyone tell me what changes I need to make in the script for 512 MB ram?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried booting the board after making changes in the imximage.cfg file but the board doesn't flash beyond u-boot.&lt;/P&gt;&lt;P&gt;These were the logs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (Sep 26 2019 - 11:25:23 +0530)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6SL rev1.2 996 MHz (running at 792 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 43C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 SoloLite EVK Board&lt;BR /&gt;Board: MX6SLEVK&lt;BR /&gt;DRAM: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even the DRAM size isn't printing now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 07:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917054#M138024</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2019-09-26T07:20:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPDDR2 Script aid for imx6sl 512 MB dram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917055#M138025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sujay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Can anyone tell me what changes I need to make in the script for 512 MB ram?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in script enter number of rows and columns according to lpddr2 datasheet.&lt;/P&gt;&lt;P&gt;Use latest ddr test:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;https://community.nxp.com/docs/DOC-105652&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For ddr test usage one can look at presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331528"&gt;DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 10:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917055#M138025</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-26T10:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPDDR2 Script aid for imx6sl 512 MB dram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917056#M138026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;I used latest stress tester and also entered rows and columns as per datasheet.&lt;/P&gt;&lt;P&gt;But still same issue persists, am I missing anything in u-boot source?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 10:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917056#M138026</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2019-09-26T10:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPDDR2 Script aid for imx6sl 512 MB dram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917057#M138027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sujay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can debug it, adding for example gpio toggle in uboot sources.&lt;/P&gt;&lt;P&gt;Check for example function dram_init():&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6slevk/mx6slevk.c?h=imx_v2017.03_4.9.88_2.0.0_ga" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6slevk/mx6slevk.c?h=imx_v2017.03_4.9.88_2.0.0_ga"&gt;mx6slevk.c\mx6slevk\freescale\board - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BTW what is exact memory size 512 MB or 512 Mb, they are both mentioned in post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 11:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-Script-aid-for-imx6sl-512-MB-dram/m-p/917057#M138027</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-26T11:03:22Z</dc:date>
    </item>
  </channel>
</rss>