<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IM8MQ using ECSPI with DMA in M4 Core.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916631#M137982</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sivaram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some examples can be found in SDK_2.6.0_EVK-MIMX8MM (I am not aware of&lt;/P&gt;&lt;P&gt;examples for i.MX8MQ), SDK can be obtained from &lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2019 21:43:53 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-06-14T21:43:53Z</dc:date>
    <item>
      <title>IM8MQ using ECSPI with DMA in M4 Core.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916630#M137981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering if there is any example or tutorial to show how to use DMA in M4 core.&lt;/P&gt;&lt;P&gt;I need to transfer 16-bit data of length 16,000 in full duplex (send and receive simultaneously) at 32MHz, for this I think the normal transfer function won't work. So I was wondering if I could use DMA but in ECSPI driver I could only find DMA Init function and also I couldn't find any driver for DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any documentation relating to this ??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 06:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916630#M137981</guid>
      <dc:creator>siva3</dc:creator>
      <dc:date>2019-06-13T06:38:29Z</dc:date>
    </item>
    <item>
      <title>Re: IM8MQ using ECSPI with DMA in M4 Core.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916631#M137982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sivaram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some examples can be found in SDK_2.6.0_EVK-MIMX8MM (I am not aware of&lt;/P&gt;&lt;P&gt;examples for i.MX8MQ), SDK can be obtained from &lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2019 21:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916631#M137982</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-14T21:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: IM8MQ using ECSPI with DMA in M4 Core.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916632#M137983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver for SDMA seems to be missing in IMX8MQ :smileysad:..Can we expect support for SDMA on IMX8MQ&amp;nbsp; anytime soon..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Sivaram SR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jun 2019 08:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916632#M137983</guid>
      <dc:creator>siva3</dc:creator>
      <dc:date>2019-06-15T08:05:09Z</dc:date>
    </item>
    <item>
      <title>Re: IM8MQ using ECSPI with DMA in M4 Core.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916633#M137984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sivaram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not think so.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jun 2019 15:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8MQ-using-ECSPI-with-DMA-in-M4-Core/m-p/916633#M137984</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-15T15:12:12Z</dc:date>
    </item>
  </channel>
</rss>