<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wlan0: Unknown error 132 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wlan0-Unknown-error-132/m-p/916295#M137924</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a document regarding to adding new WiFi card to Android OS:&lt;BR /&gt;&lt;A href="https://community.nxp.com/docs/DOC-93603" target="test_blank"&gt;https://community.nxp.com/docs/DOC-93603&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Sep 2019 01:21:10 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-09-27T01:21:10Z</dc:date>
    <item>
      <title>Wlan0: Unknown error 132</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wlan0-Unknown-error-132/m-p/916294#M137923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing issue while making wlan0 up. Below are the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have board made up from imx8mq. This board has imx8m nxp chip but the bluetooth wifi chip has been changed from qualcom to broadcom.&amp;nbsp;&lt;/P&gt;&lt;P&gt;for this.&lt;/P&gt;&lt;P&gt;1. wifi drivers has been updated&lt;/P&gt;&lt;P&gt;2. DTS files have been updated as per new interfaces.&lt;/P&gt;&lt;P&gt;Kernal version used is : 4.14.76, wifi is getting up on linux properly. The wpa_supplicant configuration file is updated for ssid and password and when the connection established successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I want same to be reflected in Android Pie, 1.0.4. (same linux kernal version 4.14.76)&lt;/P&gt;&lt;P&gt;I have followed below steps.&lt;/P&gt;&lt;P&gt;1. Wifi drivers updated as per above.&lt;/P&gt;&lt;P&gt;2. DTS files are also updated&lt;/P&gt;&lt;P&gt;3. android configuration + Buildconfig.mk updated properly&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can observe the prints for Wifi firmware to be properly installed. When I run a command for wpa_supplicant or try to up the wlan0 using ifconfig up command below error is coming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could not set interface wlan0 flags (UP): Unknown error 132&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;09-25 08:56:51.311 4234 4234 E wpa_supplicant: nl80211: Could not set interface 'wlan0' UP&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;09-25 08:56:51.311 4234 4234 I wpa_supplicant: nl80211: deinit ifname=wlan0 disabled_11b_rates=0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;09-25 08:56:51.314 4234 4234 E wpa_supplicant: wlan0: Failed to initialize driver interface&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Dmesg logs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I strace the same I got below error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ifr_flags=IFF_UP|IFF_BROADCAST|IFF_MULTICAST}) = -1 ERFKILL (Unknown error 132) &amp;lt;0.000034&amp;gt; error..&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do any one have any idea on this. Also I have obsered rfkill permission denied error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The wifi drivers are not added as kernel module instead has been updated to be as static kernel driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 08:27:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wlan0-Unknown-error-132/m-p/916294#M137923</guid>
      <dc:creator>bhumi_shah</dc:creator>
      <dc:date>2019-09-26T08:27:43Z</dc:date>
    </item>
    <item>
      <title>Re: Wlan0: Unknown error 132</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wlan0-Unknown-error-132/m-p/916295#M137924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a document regarding to adding new WiFi card to Android OS:&lt;BR /&gt;&lt;A href="https://community.nxp.com/docs/DOC-93603" target="test_blank"&gt;https://community.nxp.com/docs/DOC-93603&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 01:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wlan0-Unknown-error-132/m-p/916295#M137924</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-09-27T01:21:10Z</dc:date>
    </item>
  </channel>
</rss>