<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 NFS Error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-NFS-Error/m-p/915929#M137876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you follow the below document, especially the part where you are setting up the NFS and TFTP server in the host computer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-103717"&gt;https://community.nxp.com/docs/DOC-103717&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diego.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Sep 2019 21:28:19 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2019-09-30T21:28:19Z</dc:date>
    <item>
      <title>IMX6 NFS Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-NFS-Error/m-p/915928#M137875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;VFS: Mounted root (nfs filesystem) on device 0:17.&lt;BR /&gt;devtmpfs: mounted&lt;BR /&gt;Freeing unused kernel memory: 1024K (c1000000 - c1100000)&lt;BR /&gt;init: init first stage started!&lt;BR /&gt;audit: type=1403 audit(2434.400:2): policy loaded auid=4294967295 ses=4294967295&lt;BR /&gt;init: (Initializing SELinux non-enforcing took 0.09s.)&lt;BR /&gt;init: Sarvana : SELinux: /init&lt;BR /&gt;init: Saran : SELinux: restorecon_sb 1230&lt;BR /&gt;init: Saran : SELinux: restorecon_sb 1234&lt;BR /&gt;init: Saran : SELinux: restorecon_sb 1238&lt;BR /&gt;init: Saran : SELinux: restorecon_sb 1254&lt;BR /&gt;init: SELinux: Could not set context for /init: Operation not supported on transport endpoint&lt;BR /&gt;init: restorecon failed: Operation not supported on transport endpoint&lt;BR /&gt;init: Security failure; rebooting into recovery mode...&lt;BR /&gt;sysrq: SysRq : Emergency Remount R/O&lt;BR /&gt;Emergency Remount complete&lt;BR /&gt;reboot: Restarting system with command 'recovery'&lt;/P&gt;&lt;P&gt;U-Boot SPL 2015.04-dirty (Sep 25 2019 - 19:31:13)&lt;BR /&gt;Boot Device: SD0&lt;BR /&gt;Boot Device: SD0&lt;BR /&gt;reading u-boot.img&lt;BR /&gt;reading u-boot.img&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bootargs :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setenv ipaddr 10.17.129.68&lt;BR /&gt;setenv serverip 10.17.129.214&lt;BR /&gt;setenv nfsroot /srv/nfsandroid&lt;BR /&gt;setenv ip_dyn no&lt;BR /&gt;setenv bootfile zImage&lt;BR /&gt;setenv fdtfile imx6q-wandboard-revd1.dtb&lt;BR /&gt;setenv netargs 'setenv bootargs ${bootargs_base} console=${console},${baudrate} root=/dev/nfs rootwait rw ip=dhcp init=/init nfsroot=${serverip}:${nfsroot},v3,tcp androidboot.selinux=permissive'&lt;BR /&gt;env save&lt;BR /&gt;run netboot####&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 11:23:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-NFS-Error/m-p/915928#M137875</guid>
      <dc:creator>jgn763</dc:creator>
      <dc:date>2019-09-26T11:23:27Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 NFS Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-NFS-Error/m-p/915929#M137876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you follow the below document, especially the part where you are setting up the NFS and TFTP server in the host computer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-103717"&gt;https://community.nxp.com/docs/DOC-103717&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diego.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Sep 2019 21:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-NFS-Error/m-p/915929#M137876</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2019-09-30T21:28:19Z</dc:date>
    </item>
  </channel>
</rss>