<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question on IMX6QP Camera Input Capability</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-IMX6QP-Camera-Input-Capability/m-p/915208#M137791</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right. all these cameras can be supported by i.MX6QP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jun 2019 11:57:23 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-06-28T11:57:23Z</dc:date>
    <item>
      <title>Question on IMX6QP Camera Input Capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-IMX6QP-Camera-Input-Capability/m-p/915207#M137790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I have a question to ask regarding the data throughput of the IMX6QP camera interface.&lt;/P&gt;&lt;P&gt;I have a hardware setup as follow:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 (ONE) 3.2MP@38fps YUV422 camera connect to the IMX6QP MIPI-CS2 4 lanes port.&lt;/P&gt;&lt;P&gt;2 (TWO)&amp;nbsp; HD &lt;A href="mailto:1280x720@30fps"&gt;1280x720@30fps&lt;/A&gt;&amp;nbsp;&lt;SPAN&gt;YUV422&amp;nbsp;&lt;/SPAN&gt;cameras connect to each of the IMX6QP VIN (Parallel) ports&lt;/P&gt;&lt;P&gt;Our design target is for this setting to work in the way that the IMX6QP will read all these 3 camera simultaneously without frame drop. I have checked the Reference manual and related application notes. All in all, I am understanding that the IMX6QP can handle this setting seamlessly.&lt;/P&gt;&lt;P&gt;(My board has 64-bit DDR3 setting)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is : is my above assumption correct?! If not, what is the problem here?&lt;/P&gt;&lt;P&gt;Thank you for you time to my question.&lt;/P&gt;&lt;P&gt;Cheers,&amp;nbsp;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 07:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-IMX6QP-Camera-Input-Capability/m-p/915207#M137790</guid>
      <dc:creator>davidtrinh</dc:creator>
      <dc:date>2019-06-28T07:53:17Z</dc:date>
    </item>
    <item>
      <title>Re: Question on IMX6QP Camera Input Capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-IMX6QP-Camera-Input-Capability/m-p/915208#M137791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right. all these cameras can be supported by i.MX6QP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 11:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-IMX6QP-Camera-Input-Capability/m-p/915208#M137791</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-28T11:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: Question on IMX6QP Camera Input Capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-IMX6QP-Camera-Input-Capability/m-p/915209#M137792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;Igorpadykov,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&amp;nbsp;Highly appreciate your time.&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Jun 2019 08:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-IMX6QP-Camera-Input-Capability/m-p/915209#M137792</guid>
      <dc:creator>davidtrinh</dc:creator>
      <dc:date>2019-06-29T08:10:04Z</dc:date>
    </item>
  </channel>
</rss>