<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: About interrupt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-interrupt/m-p/915115#M137773</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Goto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for enabling / disabling gpio interrupts one can check GPIOx_ICR,&lt;/P&gt;&lt;P&gt;GPIOx_IMR registers described in sect.8.3 General Purpose Input/Output (GPIO)&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX7DRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 7Dual Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for example "Combined interrupt indication for GPIO1 signal 0 throughout 15" - if any of GPIO1(0)&lt;/P&gt;&lt;P&gt;through GPIO1(15) has enabled interrupt.&lt;/P&gt;&lt;P&gt;"Active HIGH Interrupt from INT7 from GPIO" only if GPIO1(7) interrupt is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Aug 2019 23:14:02 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-08-12T23:14:02Z</dc:date>
    <item>
      <title>About interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-interrupt/m-p/915114#M137772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the following three questions&lt;/P&gt;&lt;P&gt;About IRQ56 to IRQ63 in Table 7-1 of i.MX 7Dual Applications Processor Reference ManualI want to know the register names for enabling / disabling INT7 to INT0?&lt;/P&gt;&lt;P&gt;GPIO1 Combined interrupt indication for GPIO1 signal 0 throughout 15&lt;/P&gt;&lt;P&gt;Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?&lt;/P&gt;&lt;P&gt;Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Goto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 14:36:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-interrupt/m-p/915114#M137772</guid>
      <dc:creator>goto11</dc:creator>
      <dc:date>2019-08-12T14:36:38Z</dc:date>
    </item>
    <item>
      <title>Re: About interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-interrupt/m-p/915115#M137773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Goto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for enabling / disabling gpio interrupts one can check GPIOx_ICR,&lt;/P&gt;&lt;P&gt;GPIOx_IMR registers described in sect.8.3 General Purpose Input/Output (GPIO)&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX7DRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 7Dual Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for example "Combined interrupt indication for GPIO1 signal 0 throughout 15" - if any of GPIO1(0)&lt;/P&gt;&lt;P&gt;through GPIO1(15) has enabled interrupt.&lt;/P&gt;&lt;P&gt;"Active HIGH Interrupt from INT7 from GPIO" only if GPIO1(7) interrupt is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 23:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-interrupt/m-p/915115#M137773</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-12T23:14:02Z</dc:date>
    </item>
  </channel>
</rss>