<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: problem with package_deb in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914894#M137749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The error you are getting is error 2 that means "no such file or directory". So please check the distribution. Possibly it is incomplete because of lack of disk space.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2019 06:42:31 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-08-29T06:42:31Z</dc:date>
    <item>
      <title>problem with package_deb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914893#M137748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to&amp;nbsp;build debian package for i.MX8MQ, but it does't work. I use thud version.&lt;/P&gt;&lt;P&gt;I change local.conf file&amp;nbsp;with:&amp;nbsp;&amp;nbsp;PACKAGE_CLASSES ?= "package_deb" and EXTRA_IMAGE_FEATURES ?= "debug-tweaks package-management".&lt;/P&gt;&lt;P&gt;I try to bitbake core_image_minimal, but it&amp;nbsp;fails with this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ERROR: linux-imx-4.19.35-r0 do_package_write_deb: Fatal errors occurred in subprocesses:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Command 'PATH="/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/sources/poky/scripts:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot/usr/bin/crossscripts:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/usr/sbin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/usr/bin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/sbin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/bin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/sources/poky/bitbake/bin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/hosttools" dpkg-deb -b /home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/packages-split/kernel-module-snd-soc-bcm2835-i2s-4.19.35-imx_4.19.35_1.0.0+ge4452f4458e4 /home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/deploy-debs/imx8mqevk' returned non-zero exit status 2.: Traceback (most recent call last):&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; File "/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/sources/poky/meta/lib/oe/utils.py", line 272, in run&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; ret = self._target(*self._args, **self._kwargs)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; File "/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/sources/poky/meta/classes/package_deb.bbclass", line 274, in deb_write_pkg&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; shell=True)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; File "/usr/lib/python3.6/subprocess.py", line 356, in check_output&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; **kwargs).stdout&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; File "/usr/lib/python3.6/subprocess.py", line 438, in run&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; output=stdout, stderr=stderr)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;subprocess.CalledProcessError: Command 'PATH="/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/sources/poky/scripts:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot/usr/bin/crossscripts:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/usr/sbin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/usr/bin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/sbin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/recipe-sysroot-native/bin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/sources/poky/bitbake/bin:/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/hosttools" dpkg-deb -b /home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/packages-split/kernel-module-snd-soc-bcm2835-i2s-4.19.35-imx_4.19.35_1.0.0+ge4452f4458e4 /home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/deploy-debs/imx8mqevk' returned non-zero exit status 2.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ERROR: linux-imx-4.19.35-r0 do_package_write_deb: Function failed: do_package_deb&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ERROR: Logfile of failure stored in: /home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/build/tmp/work/imx8mqevk-poky-linux/linux-imx/4.19.35-r0/temp/log.do_package_write_deb.17810&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ERROR: Task (/home/ubuntu/yocto/imx-yocto-bsp-qt5-thud/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.19.35.bb:do_package_write_deb) failed with exit code '1'&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(points refer to similar error that I don't write here...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;someone has any idea how to solve this problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Francesco&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/package_deb in yocto/tg-p"&gt;#package_deb in yocto&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 16:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914893#M137748</guid>
      <dc:creator>francesco_giust</dc:creator>
      <dc:date>2019-08-28T16:07:59Z</dc:date>
    </item>
    <item>
      <title>Re: problem with package_deb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914894#M137749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The error you are getting is error 2 that means "no such file or directory". So please check the distribution. Possibly it is incomplete because of lack of disk space.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 06:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914894#M137749</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-08-29T06:42:31Z</dc:date>
    </item>
    <item>
      <title>Re: problem with package_deb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914895#M137750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is lot of disk space.&lt;/P&gt;&lt;P&gt;I think that problem is related to how SRCBRANCH variable is build, because introduce "_" in pkg name of kernel (e.g. kernel-module-snd-usbmidi-lib-4.19.35-imx&lt;STRONG&gt;_&lt;/STRONG&gt;4.19.35&lt;STRONG&gt;_&lt;/STRONG&gt;1.0.0+ge4452f4458e4 ) and dpkg_deb doesn't&amp;nbsp;accept this chararcter.&lt;/P&gt;&lt;P&gt;If I use package_rpm everything works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Francesco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 07:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914895#M137750</guid>
      <dc:creator>francesco_giust</dc:creator>
      <dc:date>2019-08-29T07:32:53Z</dc:date>
    </item>
    <item>
      <title>Re: problem with package_deb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914896#M137751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i don't know if you solved you problem, but we ran into exactly the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we fixed it by adding this in a linux-imx.4.19.35.bbappend file:&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;LOCALVERSION = "-${@'${SRCBRANCH}'.replace('_', '-')}"&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Laurent&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2019 13:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914896#M137751</guid>
      <dc:creator>vaudoitlaurent</dc:creator>
      <dc:date>2019-10-28T13:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: problem with package_deb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914897#M137752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Laurent,&lt;/P&gt;&lt;P&gt;yes I had already resolve the problem almost in the same way.&lt;/P&gt;&lt;P&gt;Your solution is better, I just assign a string without "_" to LOCALVERSION.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Francesco&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2019 14:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/problem-with-package-deb/m-p/914897#M137752</guid>
      <dc:creator>francesco_giust</dc:creator>
      <dc:date>2019-10-28T14:58:50Z</dc:date>
    </item>
  </channel>
</rss>