<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: ask for MIPI DSI driver code which vendor is synopsys</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913132#M137536</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;I still have two queries,please help me.&lt;/P&gt;&lt;P&gt;1.I can see such as "DRM bridge","panel bridge" "MIPI bridge" etc. in the code,so,what's the "bridge" means here,are they specified chipset?&lt;/P&gt;&lt;P&gt;2.DRM part should depend on specified chipset supporting(GPU/DPU/?)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jul 2019 03:24:37 GMT</pubDate>
    <dc:creator>guojunqiang</dc:creator>
    <dc:date>2019-07-01T03:24:37Z</dc:date>
    <item>
      <title>ask for MIPI DSI driver code which vendor is synopsys</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913130#M137534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sirs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I'm trying bring up oled panel on IMX7D chip and the MIPI DSI vendor is DWC(synopsys),&lt;/P&gt;&lt;P&gt;I just want to know whether the DWC DSI driver code is exist or not on nxp chips.&lt;/P&gt;&lt;P&gt;could you help confirm this ? if yes ,could you share the driver code ?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2019 13:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913130#M137534</guid>
      <dc:creator>guojunqiang</dc:creator>
      <dc:date>2019-06-27T13:03:01Z</dc:date>
    </item>
    <item>
      <title>Re: ask for MIPI DSI driver code which vendor is synopsys</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913131#M137535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi keil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;driver is described in sect.6.4.2 MIPI DSI Interface attached Linux Manual&lt;/P&gt;&lt;P&gt;and sources and be found in nxp linux repository&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2019 23:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913131#M137535</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-27T23:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: ask for MIPI DSI driver code which vendor is synopsys</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913132#M137536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;I still have two queries,please help me.&lt;/P&gt;&lt;P&gt;1.I can see such as "DRM bridge","panel bridge" "MIPI bridge" etc. in the code,so,what's the "bridge" means here,are they specified chipset?&lt;/P&gt;&lt;P&gt;2.DRM part should depend on specified chipset supporting(GPU/DPU/?)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2019 03:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913132#M137536</guid>
      <dc:creator>guojunqiang</dc:creator>
      <dc:date>2019-07-01T03:24:37Z</dc:date>
    </item>
    <item>
      <title>Re: ask for MIPI DSI driver code which vendor is synopsys</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913133#M137537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi keil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. "bridge"means peripheral attachment bus and used as general term in many places&lt;/P&gt;&lt;P&gt;of attached Linux Manual.&lt;/P&gt;&lt;P&gt;2. in general yes, in particular sect.6.4.1.1 Introduction Linux Manual describes:&lt;/P&gt;&lt;P&gt;"..display framework which is fbdev framework on i.MX 6 and i.MX 7 and drm framework for i.MX8. ."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2019 14:35:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913133#M137537</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-02T14:35:50Z</dc:date>
    </item>
    <item>
      <title>Re: ask for MIPI DSI driver code which vendor is synopsys</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913134#M137538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;I have checked the DWC MIPI DSI driver code you shared which is based on DRM display framework.&lt;/P&gt;&lt;P&gt;It's a pity that my code base still using fbdev model,so could you help check that driver code using fbdev model as well ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 05:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ask-for-MIPI-DSI-driver-code-which-vendor-is-synopsys/m-p/913134#M137538</guid>
      <dc:creator>guojunqiang</dc:creator>
      <dc:date>2019-07-05T05:53:38Z</dc:date>
    </item>
  </channel>
</rss>