<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8mm mipi camera csis crc error, ecc error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911820#M137400</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Qiang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first,&amp;nbsp;CRC and ECC error can be caused by poor signal, noise or low level&lt;/P&gt;&lt;P&gt;so one can check hardware using &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Mini Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also one can check &lt;A href="https://community.nxp.com/thread/463777"&gt;Explenation for HS-SETTLE  parameter in MIPI CSI D-PHY registers&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/1128143?commentID=1128143#comment-1128143" title="https://community.nxp.com/message/1128143?commentID=1128143#comment-1128143"&gt;https://community.nxp.com/message/1128143?commentID=1128143#comment-1128143&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Aug 2019 04:50:48 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-08-12T04:50:48Z</dc:date>
    <item>
      <title>imx8mm mipi camera csis crc error, ecc error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911819#M137399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using imx8mm with an mipi camera gc2145. Now camera is tramitting signals to imx8mm. I checked the status register of imx8mm mipi csi. Add debug code to read and print the value of&amp;nbsp;Interrupt source register 0 (MIPI_CSI_INTERRUPT_SOURCE_0) in mxc_mipi_csi.c, function "mipi_csis_irq_handler()".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After insmod camera driver module, use following command to capture image:&lt;/P&gt;&lt;P&gt;gst-launch-1.0 v4l2src ! jpegenc quality=50 ! filesink location=sample-gc1.jpeg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then following errrors show:&lt;/P&gt;&lt;P&gt;# gst-launch-1.0 v4l2src ! jpegenc quality=50 ! filesink location=sample-gc1.jpeg&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;[ 38.846940] [debug_xq] mipi_csis_enum_mbus_code&lt;BR /&gt;Pipeline is live and does not nee[ 38.853296] [debug_xq] mipi_csis_enum_mbus_code&lt;BR /&gt;[ 38.860843] [debug_xq] mipi_csis_enum_framesizes&lt;BR /&gt;d PREROLL ...&lt;BR /&gt;Setting pipeline t[ 38.865603] [debug_xq] mipi_csis_enum_frameintervals&lt;BR /&gt;o PLAYING ...&lt;BR /&gt;New clock: GstSyst[ 38.873503] [debug_xq] mipi_csis_enum_frameintervals&lt;BR /&gt;emClock&lt;BR /&gt;[ 38.881430] [debug_xq] mipi_csis_enum_frameintervals&lt;BR /&gt;[ 38.887243] [debug_xq] mipi_csis_enum_framesizes&lt;BR /&gt;[ 38.891982] [debug_xq] mipi_csis_enum_frameintervals&lt;BR /&gt;[ 38.897056] [debug_xq] mipi_csis_enum_frameintervals&lt;BR /&gt;[ 38.902162] [debug_xq] mipi_csis_enum_frameintervals&lt;BR /&gt;[ 38.907255] [debug_xq] mipi_csis_enum_framesizes&lt;BR /&gt;[ 38.911981] [debug_xq] mipi_csis_enum_framesizes&lt;BR /&gt;[ 38.917024] [debug_xq] mipi_csis_set_fmt&lt;BR /&gt;[ 38.921061] [debug_xq]mf-&amp;gt;code:8200, fmt-&amp;gt;colorspace:7 fmt:ffff000000dc20f0&lt;BR /&gt;[ 38.928061] [debug_xq]capturemode:0x1, mf-&amp;gt;width:1600, mf-&amp;gt;height:1200&lt;BR /&gt;[ 38.934641] [debug_xq] mipi_csis_g_parm&lt;BR /&gt;[ 38.938596] [debug_xq] mipi_csis_s_parm&lt;BR /&gt;[ 38.997722] mipi_csis_s_stream: 1, state: 0x1&lt;BR /&gt;[ 39.002114] mipi_csis_set_params: state: 0x1&lt;BR /&gt;[ 39.006518] [debug_xq] __mipi_csis_set_format&lt;BR /&gt;[ 39.011006] [debug_xq] __mipi_csis_set_format: fmt: 0x2008, 1600 x 1200&lt;BR /&gt;[ 39.017704] gc2145_mipi 2-003c: s_stream: 1&lt;BR /&gt;[ 39.021920] [debug_xq] s_stream: 1&lt;BR /&gt;[ 39.025329] stream on!&lt;BR /&gt;[ 39.035622] [debug_xq] CRC Error: 1&lt;BR /&gt;[ 39.039112] [debug_xq] Frame Start: 1&lt;BR /&gt;[ 39.042772] [debug_xq] status: 01000002&lt;BR /&gt;[ 39.046626] [debug_xq] ECC Error: 1&lt;BR /&gt;[ 39.050112] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.054041] [debug_xq] ECC Error: 2&lt;BR /&gt;[ 39.057528] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.061384] [debug_xq] CRC Error: 2&lt;BR /&gt;[ 39.064871] [debug_xq] status: 00000002&lt;BR /&gt;[ 39.068722] [debug_xq] ECC Error: 3&lt;BR /&gt;[ 39.072208] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.076059] [debug_xq] CRC Error: 3&lt;BR /&gt;[ 39.079545] [debug_xq] status: 00000002&lt;BR /&gt;[ 39.083394] [debug_xq] ECC Error: 4&lt;BR /&gt;[ 39.086881] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.097006] [debug_xq] ECC Error: 5&lt;BR /&gt;[ 39.100496] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.104356] [debug_xq] ECC Error: 6&lt;BR /&gt;[ 39.107844] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.111701] [debug_xq] CRC Error: 4&lt;BR /&gt;[ 39.115188] [debug_xq] status: 00000002&lt;BR /&gt;[ 39.119036] [debug_xq] ECC Error: 7&lt;BR /&gt;[ 39.122523] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.126430] [debug_xq] ECC Error: 8&lt;BR /&gt;[ 39.129922] [debug_xq] status: 00000004&lt;BR /&gt;[ 39.133792] [debug_xq] ECC Error: 9&lt;BR /&gt;[ 39.137283] [debug_xq] CRC Error: 5&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;I have used the same gst command to capture image with ov5640 on imx8mm EVK board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my understanding: camera image signal is transmitted into the imx8mm, but errors happens during decode the image frame.&lt;/P&gt;&lt;P&gt;What will cause the CRC and ECC error?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Xiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 02:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911819#M137399</guid>
      <dc:creator>westbrook</dc:creator>
      <dc:date>2019-08-12T02:09:42Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm mipi camera csis crc error, ecc error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911820#M137400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Qiang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first,&amp;nbsp;CRC and ECC error can be caused by poor signal, noise or low level&lt;/P&gt;&lt;P&gt;so one can check hardware using &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Mini Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also one can check &lt;A href="https://community.nxp.com/thread/463777"&gt;Explenation for HS-SETTLE  parameter in MIPI CSI D-PHY registers&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/1128143?commentID=1128143#comment-1128143" title="https://community.nxp.com/message/1128143?commentID=1128143#comment-1128143"&gt;https://community.nxp.com/message/1128143?commentID=1128143#comment-1128143&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 04:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911820#M137400</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-12T04:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm mipi camera csis crc error, ecc error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911821#M137401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick reply. I will check the link first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Xiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 05:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911821#M137401</guid>
      <dc:creator>westbrook</dc:creator>
      <dc:date>2019-08-12T05:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm mipi camera csis crc error, ecc error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911822#M137402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiao,&lt;BR /&gt;&lt;BR /&gt;I'm having almost exactly same problem with you. Did you find the root cause of the CRC and ECC errors on your board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;Efe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 15:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911822#M137402</guid>
      <dc:creator>efecan_icoz</dc:creator>
      <dc:date>2020-04-15T15:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm mipi camera csis crc error, ecc error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911823#M137403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiao:&lt;/P&gt;&lt;P&gt;I used the same camere with u. But I have not got the gc2145 driver code . Can you share your driver code to me ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 07:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-mipi-camera-csis-crc-error-ecc-error/m-p/911823#M137403</guid>
      <dc:creator>rongyong_deng</dc:creator>
      <dc:date>2020-08-10T07:41:25Z</dc:date>
    </item>
  </channel>
</rss>