<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX sdma-imx7d.bin licensing issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911193#M137324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markus,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your response. I also tried to compile the spi-imx as module but it didn't work as expected since its still loading the rom firmware and not the binary which is located in the rootfs (/lib/firmware/imx/sdma).&lt;/P&gt;&lt;P&gt;Are there any more modifications I have to do getting the devices on the SPI working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Christoph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Sep 2019 12:12:53 GMT</pubDate>
    <dc:creator>c_freiberger</dc:creator>
    <dc:date>2019-09-13T12:12:53Z</dc:date>
    <item>
      <title>IMX sdma-imx7d.bin licensing issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911189#M137320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it possible to load the sdma-imx7d.bin firmware binary from userspace /lib/firmware...&lt;/P&gt;&lt;P&gt;I don"t want to put it in the Kernel in perspective of not violating gplv2 terms with including it in the Kernel.&lt;/P&gt;&lt;P&gt;Any help would be appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 14:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911189#M137320</guid>
      <dc:creator>c_freiberger</dc:creator>
      <dc:date>2019-08-27T14:22:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX sdma-imx7d.bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911190#M137321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christoph,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use sdma-imx7d.bin firmware in another kernel version that is not supported by NXP you can use it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 15:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911190#M137321</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-08-28T15:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX sdma-imx7d.bin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911191#M137322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yeah, but since compiling properitary licenced modules into your kernel binary violates the GPLv2 licence of the kernel itself.&lt;/P&gt;&lt;P&gt;Therefor I am asking if there is a way to invoke the SDMA firmware from userspace since i didn't get it running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 08:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911191#M137322</guid>
      <dc:creator>c_freiberger</dc:creator>
      <dc:date>2019-09-02T08:47:34Z</dc:date>
    </item>
    <item>
      <title>Re: IMX sdma-imx7d.bin licensing issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911192#M137323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christoph,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it's possible and it works for us - the firmware is also in the linux-firmware repo. To load the firmware from userspace, you need to compile the SDMA driver as a module. Then the driver will load the firmware when it binds to the SDMA. Depending on your usecase, audio drivers that use SDMA are also a candidate to be compiled as module.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 17:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911192#M137323</guid>
      <dc:creator>Niebel-TQ</dc:creator>
      <dc:date>2019-09-12T17:35:58Z</dc:date>
    </item>
    <item>
      <title>Re: IMX sdma-imx7d.bin licensing issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911193#M137324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markus,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your response. I also tried to compile the spi-imx as module but it didn't work as expected since its still loading the rom firmware and not the binary which is located in the rootfs (/lib/firmware/imx/sdma).&lt;/P&gt;&lt;P&gt;Are there any more modifications I have to do getting the devices on the SPI working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Christoph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2019 12:12:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-sdma-imx7d-bin-licensing-issue/m-p/911193#M137324</guid>
      <dc:creator>c_freiberger</dc:creator>
      <dc:date>2019-09-13T12:12:53Z</dc:date>
    </item>
  </channel>
</rss>