<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Reboot failed -- System halted(imx6q) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910652#M137219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you don't have PMIC you can't use the external reset.&lt;/P&gt;&lt;P&gt;In this case keep wdog1 enabled and wdog2 disabled, which is the default configuration for imx6qdl.dtsi:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=imx_5.4.3_2.0.0#n748" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=imx_5.4.3_2.0.0#n748"&gt;imx6qdl.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is overriden in SABRE SD EVK dts:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_5.4.3_2.0.0#n1186" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_5.4.3_2.0.0#n1186"&gt;imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&lt;/P&gt;&lt;P&gt;so you need to make sure wdog1 and wdog2 configuration from imx6qdl.dtsi is not overridden somewhere in your board dts hierarchy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Aug 2020 19:32:03 GMT</pubDate>
    <dc:creator>DiegoFSL</dc:creator>
    <dc:date>2020-08-14T19:32:03Z</dc:date>
    <item>
      <title>Reboot failed -- System halted(imx6q)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910649#M137216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 18.684772] reboot: Restarting system&lt;BR /&gt;[ 18.688457] CPU: 0 PID: 440 Comm: reboot Not tainted 4.9.11-1.0.0+gc27010d99a3d #6&lt;BR /&gt;[ 18.696032] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)&lt;BR /&gt;[ 18.702597] [&amp;lt;8010f954&amp;gt;] (unwind_backtrace) from [&amp;lt;8010b398&amp;gt;] (show_stack+0x10/0x14)&lt;BR /&gt;[ 18.710359] [&amp;lt;8010b398&amp;gt;] (show_stack) from [&amp;lt;803c0918&amp;gt;] (dump_stack+0x78/0x8c)&lt;BR /&gt;[ 18.717597] [&amp;lt;803c0918&amp;gt;] (dump_stack) from [&amp;lt;80109ac0&amp;gt;] (machine_restart+0xc/0x80)&lt;BR /&gt;[ 18.725181] [&amp;lt;80109ac0&amp;gt;] (machine_restart) from [&amp;lt;8014c640&amp;gt;] (SyS_reboot+0xc8/0x1ac)&lt;BR /&gt;[ 18.732937] [&amp;lt;8014c640&amp;gt;] (SyS_reboot) from [&amp;lt;80107880&amp;gt;] (ret_fast_syscall+0x0/0x3c)&lt;BR /&gt;&lt;STRONG style="color: #ff0000; "&gt;[ 18.840659] imx2-wdt 20c0000.wdog: failed to assert external reset, trying with timeout&lt;/STRONG&gt;&lt;BR /&gt;[ 19.848669] Reboot failed -- System halted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 09:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910649#M137216</guid>
      <dc:creator>1042484520</dc:creator>
      <dc:date>2019-08-27T09:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: Reboot failed -- System halted(imx6q)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910650#M137217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello qingzong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Try removing the pfuze100 from the kernel, and see that it can be boot up&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 15:03:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910650#M137217</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-08-28T15:03:55Z</dc:date>
    </item>
    <item>
      <title>Re: Reboot failed -- System halted(imx6q)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910651#M137218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bio:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Still can't restart after removal.&lt;/P&gt;&lt;P&gt;Thx!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 10:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910651#M137218</guid>
      <dc:creator>1042484520</dc:creator>
      <dc:date>2019-08-29T10:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: Reboot failed -- System halted(imx6q)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910652#M137219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you don't have PMIC you can't use the external reset.&lt;/P&gt;&lt;P&gt;In this case keep wdog1 enabled and wdog2 disabled, which is the default configuration for imx6qdl.dtsi:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=imx_5.4.3_2.0.0#n748" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=imx_5.4.3_2.0.0#n748"&gt;imx6qdl.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is overriden in SABRE SD EVK dts:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_5.4.3_2.0.0#n1186" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_5.4.3_2.0.0#n1186"&gt;imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&lt;/P&gt;&lt;P&gt;so you need to make sure wdog1 and wdog2 configuration from imx6qdl.dtsi is not overridden somewhere in your board dts hierarchy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2020 19:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reboot-failed-System-halted-imx6q/m-p/910652#M137219</guid>
      <dc:creator>DiegoFSL</dc:creator>
      <dc:date>2020-08-14T19:32:03Z</dc:date>
    </item>
  </channel>
</rss>