<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What happens to the boot sequence when CA53 Core0 is software reset? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910256#M137136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;yes. But there is chance that it will hang, as ROM expects POR reset (so whole processor is ready to boot).&lt;/BLOCKQUOTE&gt;&lt;P&gt;As a reminder, if CM4 resets Core0 with A53_CORE_RESET0, will the CM4 core be affected? ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;T.Kashiwagi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Aug 2019 15:08:32 GMT</pubDate>
    <dc:creator>Takashi_Kashiwagi</dc:creator>
    <dc:date>2019-08-13T15:08:32Z</dc:date>
    <item>
      <title>What happens to the boot sequence when CA53 Core0 is software reset?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910252#M137132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read 6.1 System Boot in the IMX8MM reference manual, but I didn't understand the behavior when resetting the software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use CM4 Core for&amp;nbsp;alive monitoring of CA53.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to RM, the SRC_A53RCR0 can be used to reset the CA53 core, but I could not understand what the boot sequence would be when the Core0 was software reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it the same sequence as POR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;（It was useful if there was a boot option that would start from CM4 at POR......）&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;T.Kashiwagi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Aug 2019 14:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910252#M137132</guid>
      <dc:creator>Takashi_Kashiwagi</dc:creator>
      <dc:date>2019-08-11T14:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: What happens to the boot sequence when CA53 Core0 is software reset?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910253#M137133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kashiwagi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;According to RM, the SRC_A53RCR0 can be used to reset the CA53 core, but I could&lt;/P&gt;&lt;P&gt;&amp;gt;not understand what the boot sequence would be when the Core0 was software reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;strictly speaking only resetting the CA53 core may not be sufficient for successful boot,&lt;/P&gt;&lt;P&gt;as boot ROM expects that other processor modules were in predefined (reset) state.&lt;/P&gt;&lt;P&gt;Such state is provided only using POR, as described in sect.6.5.4.1.2.1 POR (SRC_POR_B)&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Mini Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;It was useful if there was a boot option that would start from CM4 at POR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sorry this is not possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 01:50:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910253#M137133</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-12T01:50:58Z</dc:date>
    </item>
    <item>
      <title>Re: What happens to the boot sequence when CA53 Core0 is software reset?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910254#M137134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for responding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;strictly speaking only resetting the CA53 core may not be sufficient for successful boot,&lt;/P&gt;&lt;P&gt;as boot ROM expects that other processor modules were in predefined (reset) state.&lt;/P&gt;&lt;P&gt;Such state is provided only using POR, as described in sect.6.5.4.1.2.1 POR (SRC_POR_B)&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;It seems that all cores are reset when POR is reset. I don't want to reset the CM4 core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is written that A53_CORE_RESET0 of SRC_A53RCR0 register resets only Core0.&lt;/P&gt;&lt;P&gt;If I reset CA0 Core0 from CM4 using this bit, &lt;STRONG&gt;will Core0 start from boot ROM (0x00000000)?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My ideal is as follows.&lt;BR /&gt;・ When resetting CA53 Core0, &lt;STRONG&gt;CM4 core does not want to be reset&lt;/STRONG&gt;.&lt;BR /&gt;・ When I reset the CA53 core from the CM4 core, I want to start the CA53 core with u-boot-spl.bin or u-boot.img loaded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;T.Kashiwagi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 14:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910254#M137134</guid>
      <dc:creator>Takashi_Kashiwagi</dc:creator>
      <dc:date>2019-08-12T14:54:06Z</dc:date>
    </item>
    <item>
      <title>Re: What happens to the boot sequence when CA53 Core0 is software reset?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910255#M137135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kashiwagi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;If I reset CA0 Core0 from CM4 using this bit, will Core0 start from boot ROM (0x00000000)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes. But there is chance that it will hang, as ROM expects POR reset (so whole processor is ready to boot).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 15:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910255#M137135</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-12T15:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: What happens to the boot sequence when CA53 Core0 is software reset?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910256#M137136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;yes. But there is chance that it will hang, as ROM expects POR reset (so whole processor is ready to boot).&lt;/BLOCKQUOTE&gt;&lt;P&gt;As a reminder, if CM4 resets Core0 with A53_CORE_RESET0, will the CM4 core be affected? ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;T.Kashiwagi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2019 15:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910256#M137136</guid>
      <dc:creator>Takashi_Kashiwagi</dc:creator>
      <dc:date>2019-08-13T15:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: What happens to the boot sequence when CA53 Core0 is software reset?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910257#M137137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kashiwagi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;if CM4 resets Core0 with A53_CORE_RESET0, will the CM4 core be affected?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2019 15:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-to-the-boot-sequence-when-CA53-Core0-is-software/m-p/910257#M137137</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-13T15:14:10Z</dc:date>
    </item>
  </channel>
</rss>