<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLower CPU frequency on imx8mq</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/909502#M137030</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the latest release 4.9.98_2.0.0 on iMX 8M Quad EVK.&lt;/P&gt;&lt;P&gt;I want to set the CPU frequency lower than 1.0GHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to change the dts file with i.MX_Linux Reference_Manual.pdf, but there are 4 operational points already.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;~/imx-yocto-bsp/build-xwayland/tmp/work-shared/imx8mqevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mq-evk.dts&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;amp;A53_0 {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;operating-points = &amp;lt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;/* kHz uV */&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;1500000 1000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;1300000 1000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;1000000 900000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;800000 900000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;dc-supply = &amp;lt;&amp;amp;reg_gpio_dvfs&amp;gt;;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;};&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I confirmed that the EVK board is using this dts.&lt;BR /&gt;&lt;EM&gt;root@imx8mqevk:/proc/device-tree# strings compatible&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fsl,imx8mq-evk&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fsl,imx8mq&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The operating point is displayed as follows.&lt;BR /&gt;&lt;EM&gt;root@imx8mqevk:/proc/device-tree/cpus/cpu@0# hexdump -C operating-points&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;00000000 00 16 e3 60 00 0f 42 40 00 13 d6 20 00 0f 42 40 |...`..B@... ..B@|&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;00000010 00 0f 42 40 00 0d bb a0 00 0c 35 00 00 0d bb a0 |..B@......5.....|&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x16e360 -&amp;gt; 1500000(1.5GHz)&lt;BR /&gt;0x13d620 -&amp;gt; 1300000(1.3GHz)&lt;BR /&gt;0xf4240 -&amp;gt; 1000000(1.0GHz)&lt;BR /&gt;0xdbba0 -&amp;gt; 900000(900MHz)&lt;BR /&gt;0xc3500 -&amp;gt; 800000(800MHz)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;However, only two operating points in the governor are displayed.&lt;BR /&gt;&lt;EM&gt;root@imx8mqevk:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_available_frequencies&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1000000 1500000&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the minimum clock cannot be set lower than 1.0GHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where should I change to add an operating point?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Yoshinari.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2019 06:43:59 GMT</pubDate>
    <dc:creator>daisukeyoshinar</dc:creator>
    <dc:date>2019-08-29T06:43:59Z</dc:date>
    <item>
      <title>Lower CPU frequency on imx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/909502#M137030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the latest release 4.9.98_2.0.0 on iMX 8M Quad EVK.&lt;/P&gt;&lt;P&gt;I want to set the CPU frequency lower than 1.0GHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to change the dts file with i.MX_Linux Reference_Manual.pdf, but there are 4 operational points already.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;~/imx-yocto-bsp/build-xwayland/tmp/work-shared/imx8mqevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mq-evk.dts&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;amp;A53_0 {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;operating-points = &amp;lt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;/* kHz uV */&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;1500000 1000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;1300000 1000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;1000000 900000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;800000 900000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;dc-supply = &amp;lt;&amp;amp;reg_gpio_dvfs&amp;gt;;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;};&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I confirmed that the EVK board is using this dts.&lt;BR /&gt;&lt;EM&gt;root@imx8mqevk:/proc/device-tree# strings compatible&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fsl,imx8mq-evk&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fsl,imx8mq&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The operating point is displayed as follows.&lt;BR /&gt;&lt;EM&gt;root@imx8mqevk:/proc/device-tree/cpus/cpu@0# hexdump -C operating-points&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;00000000 00 16 e3 60 00 0f 42 40 00 13 d6 20 00 0f 42 40 |...`..B@... ..B@|&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;00000010 00 0f 42 40 00 0d bb a0 00 0c 35 00 00 0d bb a0 |..B@......5.....|&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x16e360 -&amp;gt; 1500000(1.5GHz)&lt;BR /&gt;0x13d620 -&amp;gt; 1300000(1.3GHz)&lt;BR /&gt;0xf4240 -&amp;gt; 1000000(1.0GHz)&lt;BR /&gt;0xdbba0 -&amp;gt; 900000(900MHz)&lt;BR /&gt;0xc3500 -&amp;gt; 800000(800MHz)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;However, only two operating points in the governor are displayed.&lt;BR /&gt;&lt;EM&gt;root@imx8mqevk:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_available_frequencies&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1000000 1500000&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the minimum clock cannot be set lower than 1.0GHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where should I change to add an operating point?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Yoshinari.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 06:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/909502#M137030</guid>
      <dc:creator>daisukeyoshinar</dc:creator>
      <dc:date>2019-08-29T06:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: Lower CPU frequency on imx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/909503#M137031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yoshinari&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these operating points are for both industrial and consumer gardes, while&lt;/P&gt;&lt;P&gt;consumer grade supports only 1.GHz, 1.5GHz according to Table 7. Operating ranges&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX8MDQLQCEC.pdf" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Dual / 8M QuadLite / 8M Quad Applications Processors Data Sheet for Consumer Products&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;industrial grade supports only 800MHz, 1.3GHz according to Table 7. Operating ranges&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX8MDQLQIEC.pdf" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Dual / 8M QuadLite / 8M Quad Applications Processors Data Sheet for Industrial Products&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;gt;Where should I change to add an operating point?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for other frequencies one will have to modify cpufreq driver described in sect.2.3.3.2.1 Source Code Structure&lt;/P&gt;&lt;P&gt;attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 11:06:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/909503#M137031</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-29T11:06:57Z</dc:date>
    </item>
    <item>
      <title>Re: Lower CPU frequency on imx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/909504#M137032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The operating point was disabled by grade.&lt;BR /&gt;&lt;EM&gt;/imx8mqevk/kernel-source/drivers/soc/imx/soc-imx8.c&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After changing, it became 800MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daisuke Yoshinari&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Aug 2019 08:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/909504#M137032</guid>
      <dc:creator>daisukeyoshinar</dc:creator>
      <dc:date>2019-08-30T08:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: Lower CPU frequency on imx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/1435315#M188718</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Are you saying that it is possible to create our own operating points which can be of a frequency below the frequencies mentioned in the data sheet by adding to the OPP tables in the correct dtsi file in&amp;nbsp;arch/arm/boot/dts? Or do we modify the actual NXP&amp;nbsp;&lt;SPAN&gt;cpufreq driver in the correct imx*-cpufreq.c file to create some custom frequency? Is that even possible? For example, if on my i.MX8DXP the only available frequencies in cpufreq are 900000 kHZ and 1200000 kHz, how can I create a setting to go even lower?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Mar 2022 07:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mq/m-p/1435315#M188718</guid>
      <dc:creator>yhegde</dc:creator>
      <dc:date>2022-03-29T07:34:58Z</dc:date>
    </item>
  </channel>
</rss>