<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBuild an IMX yocto image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Build-an-IMX-yocto-image/m-p/908893#M136966</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a very specific board based on imx287 and I'm trying to build an image with yocto.&lt;/P&gt;&lt;P&gt;I know how to use yocto basically (build an ixm28evk board 's image for instance) and how to build new layer,... but I'm lost when I try to configure the layer to fit my board.&lt;/P&gt;&lt;P&gt;That I know and that I have regarding my board:&lt;/P&gt;&lt;P&gt;- I have the .dtb file&lt;/P&gt;&lt;P&gt;- My board doesn't use u-boot as bootloader but imx-bootlet (how can I use imx instead of uboot? and is it necessary?)&lt;/P&gt;&lt;P&gt;- I know the partitions' size&lt;/P&gt;&lt;P&gt;- I need the MFGTool to flash the board&lt;/P&gt;&lt;P&gt;- the kernel configuration file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I produce a zimage (MFGTool compatible) with my own device tree and the bootloader imx-bootlet?&lt;/P&gt;&lt;P&gt;Thanks for your help :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jun 2019 15:42:16 GMT</pubDate>
    <dc:creator>alexoubj</dc:creator>
    <dc:date>2019-06-11T15:42:16Z</dc:date>
    <item>
      <title>Build an IMX yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-an-IMX-yocto-image/m-p/908893#M136966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a very specific board based on imx287 and I'm trying to build an image with yocto.&lt;/P&gt;&lt;P&gt;I know how to use yocto basically (build an ixm28evk board 's image for instance) and how to build new layer,... but I'm lost when I try to configure the layer to fit my board.&lt;/P&gt;&lt;P&gt;That I know and that I have regarding my board:&lt;/P&gt;&lt;P&gt;- I have the .dtb file&lt;/P&gt;&lt;P&gt;- My board doesn't use u-boot as bootloader but imx-bootlet (how can I use imx instead of uboot? and is it necessary?)&lt;/P&gt;&lt;P&gt;- I know the partitions' size&lt;/P&gt;&lt;P&gt;- I need the MFGTool to flash the board&lt;/P&gt;&lt;P&gt;- the kernel configuration file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I produce a zimage (MFGTool compatible) with my own device tree and the bootloader imx-bootlet?&lt;/P&gt;&lt;P&gt;Thanks for your help :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 15:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-an-IMX-yocto-image/m-p/908893#M136966</guid>
      <dc:creator>alexoubj</dc:creator>
      <dc:date>2019-06-11T15:42:16Z</dc:date>
    </item>
    <item>
      <title>Re: Build an IMX yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-an-IMX-yocto-image/m-p/908894#M136967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the mfgtool firmware, you can refer to this&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/1042399" shape="rect" target="_blank"&gt;https://community.nxp.com/message/1042399&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2019 04:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-an-IMX-yocto-image/m-p/908894#M136967</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2019-06-14T04:29:04Z</dc:date>
    </item>
  </channel>
</rss>