<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 build does not create an SDCard image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/build-does-not-create-an-SDCard-image/m-p/908554#M136935</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello.&lt;/P&gt;&lt;P&gt;i am trying to create an image for imx8mq. i will print my history commands&lt;/P&gt;&lt;P&gt;1912 DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-xwayland&lt;BR /&gt;1927 bitbake fsl-image-qt5-validation-imx&lt;BR /&gt;build output&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WARNING: Host distribution "ubuntu-18.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.&lt;BR /&gt;Loading cache: 100% |###############################################################################################################################################################################| Time: 0:00:00&lt;BR /&gt;Loaded 3260 entries from dependency cache.&lt;BR /&gt;Parsing recipes: 100% |#############################################################################################################################################################################| Time: 0:00:01&lt;BR /&gt;Parsing of 2423 .bb files complete (2419 cached, 4 parsed). 3264 targets, 212 skipped, 8 masked, 0 errors.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.36.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-18.04"&lt;BR /&gt;TARGET_SYS = "aarch64-poky-linux"&lt;BR /&gt;MACHINE = "imx8mqevk"&lt;BR /&gt;DISTRO = "fsl-imx-xwayland"&lt;BR /&gt;DISTRO_VERSION = "4.9.88-2.0.0"&lt;BR /&gt;TUNE_FEATURES = "aarch64"&lt;BR /&gt;TARGET_FPU = ""&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:0ec241873367e18f5371a3ad9aca1e2801dcd4ee"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-freescale = "HEAD:49ac225a38f6d84519798e3264f2e4d19b84f70a"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:1d6d5961dbf82624b28bb318b4950a64abc31d12"&lt;BR /&gt;meta-freescale-distro = "HEAD:0ec6d7e206705702b5b534611754de0787f92b72"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk = "HEAD:d65692ecb3a4136fc1cc137152634e8633ddb3c6"&lt;BR /&gt;meta-browser = "HEAD:d6f9aed41c73b75a97d71bff060b03a66ee087b1"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-python &lt;BR /&gt;meta-filesystems = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-qt5 = "HEAD:32bb7d18a08d1c48873d7ab6332d4cc3815a4dff"&lt;/P&gt;&lt;P&gt;Initialising tasks: 100% |##########################################################################################################################################################################| Time: 0:00:10&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: QA Issue: /lib/firmware/murata/.git/hooks/fsmonitor-watchman.sample contained in package linux-firmware requires /usr/bin/perl, but no providers found in RDEPENDS_linux-firmware? [file-rdeps]&lt;BR /&gt;ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.&lt;BR /&gt;ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: Function failed: do_package_qa&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/elsec-linux/build/imx-yocto-bsp/build-xwayland/tmp/work/all-poky-linux/linux-firmware/1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0/temp/log.do_package_qa.31317&lt;BR /&gt;ERROR: Task (/home/elsec-linux/build/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 6994 tasks of which 6978 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt; /home/elsec-linux/build/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There were 3 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i look at the images directory (fsl-image-qt5-validation-imx)&lt;/P&gt;&lt;P&gt;i do not see an sdcard image.&lt;/P&gt;&lt;P&gt;is the image not created because of the errors in the build or because of a bad configuration&amp;nbsp;&lt;/P&gt;&lt;P&gt;my build/conf/local.conf&lt;/P&gt;&lt;P&gt;MACHINE ??= 'imx8mqevk'&lt;BR /&gt;DISTRO ?= 'fsl-imx-xwayland'&lt;BR /&gt;PACKAGE_CLASSES ?= "package_rpm"&lt;BR /&gt;EXTRA_IMAGE_FEATURES ?= "debug-tweaks"&lt;BR /&gt;USER_CLASSES ?= "buildstats image-mklibs image-prelink"&lt;BR /&gt;PATCHRESOLVE = "noop"&lt;/P&gt;&lt;P&gt;TOOLCHAIN_TARGET_TASK_append = " gtk+ gtk+3"&lt;BR /&gt;IMAGE_INSTALL_append = " gtk+ gtk+3"&lt;BR /&gt;BB_DISKMON_DIRS ??= "\&lt;BR /&gt; STOPTASKS,${TMPDIR},1G,100K \&lt;BR /&gt; STOPTASKS,${DL_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,${SSTATE_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,/tmp,100M,100K \&lt;BR /&gt; ABORT,${TMPDIR},100M,1K \&lt;BR /&gt; ABORT,${DL_DIR},100M,1K \&lt;BR /&gt; ABORT,${SSTATE_DIR},100M,1K \&lt;BR /&gt; ABORT,/tmp,10M,1K"&lt;BR /&gt;PACKAGECONFIG_append_pn-qemu-native = " sdl"&lt;BR /&gt;PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"&lt;BR /&gt;CONF_VERSION = "1"&lt;/P&gt;&lt;P&gt;DL_DIR ?= "${BSPDIR}/downloads/"&lt;BR /&gt;ACCEPT_FSL_EULA = "1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 11 Aug 2019 11:01:28 GMT</pubDate>
    <dc:creator>greeranjunk</dc:creator>
    <dc:date>2019-08-11T11:01:28Z</dc:date>
    <item>
      <title>build does not create an SDCard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/build-does-not-create-an-SDCard-image/m-p/908554#M136935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello.&lt;/P&gt;&lt;P&gt;i am trying to create an image for imx8mq. i will print my history commands&lt;/P&gt;&lt;P&gt;1912 DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-xwayland&lt;BR /&gt;1927 bitbake fsl-image-qt5-validation-imx&lt;BR /&gt;build output&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WARNING: Host distribution "ubuntu-18.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.&lt;BR /&gt;Loading cache: 100% |###############################################################################################################################################################################| Time: 0:00:00&lt;BR /&gt;Loaded 3260 entries from dependency cache.&lt;BR /&gt;Parsing recipes: 100% |#############################################################################################################################################################################| Time: 0:00:01&lt;BR /&gt;Parsing of 2423 .bb files complete (2419 cached, 4 parsed). 3264 targets, 212 skipped, 8 masked, 0 errors.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.36.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-18.04"&lt;BR /&gt;TARGET_SYS = "aarch64-poky-linux"&lt;BR /&gt;MACHINE = "imx8mqevk"&lt;BR /&gt;DISTRO = "fsl-imx-xwayland"&lt;BR /&gt;DISTRO_VERSION = "4.9.88-2.0.0"&lt;BR /&gt;TUNE_FEATURES = "aarch64"&lt;BR /&gt;TARGET_FPU = ""&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:0ec241873367e18f5371a3ad9aca1e2801dcd4ee"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-freescale = "HEAD:49ac225a38f6d84519798e3264f2e4d19b84f70a"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:1d6d5961dbf82624b28bb318b4950a64abc31d12"&lt;BR /&gt;meta-freescale-distro = "HEAD:0ec6d7e206705702b5b534611754de0787f92b72"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk = "HEAD:d65692ecb3a4136fc1cc137152634e8633ddb3c6"&lt;BR /&gt;meta-browser = "HEAD:d6f9aed41c73b75a97d71bff060b03a66ee087b1"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-python &lt;BR /&gt;meta-filesystems = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"&lt;BR /&gt;meta-qt5 = "HEAD:32bb7d18a08d1c48873d7ab6332d4cc3815a4dff"&lt;/P&gt;&lt;P&gt;Initialising tasks: 100% |##########################################################################################################################################################################| Time: 0:00:10&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: QA Issue: /lib/firmware/murata/.git/hooks/fsmonitor-watchman.sample contained in package linux-firmware requires /usr/bin/perl, but no providers found in RDEPENDS_linux-firmware? [file-rdeps]&lt;BR /&gt;ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.&lt;BR /&gt;ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: Function failed: do_package_qa&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/elsec-linux/build/imx-yocto-bsp/build-xwayland/tmp/work/all-poky-linux/linux-firmware/1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0/temp/log.do_package_qa.31317&lt;BR /&gt;ERROR: Task (/home/elsec-linux/build/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 6994 tasks of which 6978 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt; /home/elsec-linux/build/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There were 3 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i look at the images directory (fsl-image-qt5-validation-imx)&lt;/P&gt;&lt;P&gt;i do not see an sdcard image.&lt;/P&gt;&lt;P&gt;is the image not created because of the errors in the build or because of a bad configuration&amp;nbsp;&lt;/P&gt;&lt;P&gt;my build/conf/local.conf&lt;/P&gt;&lt;P&gt;MACHINE ??= 'imx8mqevk'&lt;BR /&gt;DISTRO ?= 'fsl-imx-xwayland'&lt;BR /&gt;PACKAGE_CLASSES ?= "package_rpm"&lt;BR /&gt;EXTRA_IMAGE_FEATURES ?= "debug-tweaks"&lt;BR /&gt;USER_CLASSES ?= "buildstats image-mklibs image-prelink"&lt;BR /&gt;PATCHRESOLVE = "noop"&lt;/P&gt;&lt;P&gt;TOOLCHAIN_TARGET_TASK_append = " gtk+ gtk+3"&lt;BR /&gt;IMAGE_INSTALL_append = " gtk+ gtk+3"&lt;BR /&gt;BB_DISKMON_DIRS ??= "\&lt;BR /&gt; STOPTASKS,${TMPDIR},1G,100K \&lt;BR /&gt; STOPTASKS,${DL_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,${SSTATE_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,/tmp,100M,100K \&lt;BR /&gt; ABORT,${TMPDIR},100M,1K \&lt;BR /&gt; ABORT,${DL_DIR},100M,1K \&lt;BR /&gt; ABORT,${SSTATE_DIR},100M,1K \&lt;BR /&gt; ABORT,/tmp,10M,1K"&lt;BR /&gt;PACKAGECONFIG_append_pn-qemu-native = " sdl"&lt;BR /&gt;PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"&lt;BR /&gt;CONF_VERSION = "1"&lt;/P&gt;&lt;P&gt;DL_DIR ?= "${BSPDIR}/downloads/"&lt;BR /&gt;ACCEPT_FSL_EULA = "1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Aug 2019 11:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/build-does-not-create-an-SDCard-image/m-p/908554#M136935</guid>
      <dc:creator>greeranjunk</dc:creator>
      <dc:date>2019-08-11T11:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: build does not create an SDCard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/build-does-not-create-an-SDCard-image/m-p/908555#M136936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i found the problem. i had an error with my build and i assumed that the build continued. the error was because i am using a new Ubuntu version. after i fix the error the sdcard image was created&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 06:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/build-does-not-create-an-SDCard-image/m-p/908555#M136936</guid>
      <dc:creator>greeranjunk</dc:creator>
      <dc:date>2019-08-12T06:13:52Z</dc:date>
    </item>
    <item>
      <title>Re: build does not create an SDCard image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/build-does-not-create-an-SDCard-image/m-p/908556#M136937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, maybe you should use ubutun 16.04 instead of 18.04&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 09:16:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/build-does-not-create-an-SDCard-image/m-p/908556#M136937</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-08-12T09:16:40Z</dc:date>
    </item>
  </channel>
</rss>