<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: GPU driver crash on i.MX8M-Mini with 4GB RAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/908461#M136913</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;Hello,&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp; According to section 2.1.2 (Cortex-A53 Memory Map) of i.MX 8M Mini&amp;nbsp; Reference Manual,&lt;/P&gt;&lt;P class=""&gt;Rev. 1, 03/2019, only 3072MB of DDR Memory address area&amp;nbsp; are available for all modules,&lt;/P&gt;&lt;P class=""&gt;including GPU. But address range, starting from 0x1_0000_0000 is accessible only&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;by the ARM Cores.&amp;nbsp; This provides problem for NXP Linux, in particular for GPU DMA. &amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2019 11:26:49 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2019-06-14T11:26:49Z</dc:date>
    <item>
      <title>GPU driver crash on i.MX8M-Mini with 4GB RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/908460#M136912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're experiencing GPU driver (galcore) crash on our i.MX8M-Mini board with 4GB of RAM running latest NXP BSP 4.14.98-2.0.1. Restricting memory size to 3GB by passing mem=3G kernel command line parameter fixes the problem. Is this a known problem ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Felix.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 10:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/908460#M136912</guid>
      <dc:creator>felixradensky</dc:creator>
      <dc:date>2019-06-11T10:17:55Z</dc:date>
    </item>
    <item>
      <title>Re: GPU driver crash on i.MX8M-Mini with 4GB RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/908461#M136913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;Hello,&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp; According to section 2.1.2 (Cortex-A53 Memory Map) of i.MX 8M Mini&amp;nbsp; Reference Manual,&lt;/P&gt;&lt;P class=""&gt;Rev. 1, 03/2019, only 3072MB of DDR Memory address area&amp;nbsp; are available for all modules,&lt;/P&gt;&lt;P class=""&gt;including GPU. But address range, starting from 0x1_0000_0000 is accessible only&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;by the ARM Cores.&amp;nbsp; This provides problem for NXP Linux, in particular for GPU DMA. &amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2019 11:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/908461#M136913</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-06-14T11:26:49Z</dc:date>
    </item>
    <item>
      <title>Re: GPU driver crash on i.MX8M-Mini with 4GB RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/908462#M136914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri&lt;/P&gt;&lt;P&gt;The following patch: &lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/commit/drivers/mxc/gpu-viv?h=imx_4.14.98_2.0.0_ga&amp;amp;id=05ed5881e67984e0c5170a5272cb7afb4afadf83" title="https://source.codeaurora.org/external/imx/linux-imx/commit/drivers/mxc/gpu-viv?h=imx_4.14.98_2.0.0_ga&amp;amp;id=05ed5881e67984e0c5170a5272cb7afb4afadf83"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp; fixed GPU memory access for i.MX8M but missed to do the same for i.MX8M Mini. Adding check for "fsl,imx8mm-gpu" fixes the crash on Mini.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Felix.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jun 2019 08:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/908462#M136914</guid>
      <dc:creator>felixradensky</dc:creator>
      <dc:date>2019-06-15T08:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: GPU driver crash on i.MX8M-Mini with 4GB RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/1729012#M213115</link>
      <description>&lt;P&gt;Hi, Even this issues still persist in kernel v5.15.71 in NXP BSP - kirkstone branch.&lt;BR /&gt;&lt;BR /&gt;We faced it with one of our customer for sway compositor.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;[   27.464790] etnaviv-gpu 38000000.gpu: AXI bus error&lt;/SPAN&gt;
&lt;SPAN class=""&gt;[   27.469745] etnaviv-gpu 38000000.gpu: MMU fault status 0x00000000&lt;/SPAN&gt;
&lt;SPAN class=""&gt;[   27.970450] etnaviv-gpu 38000000.gpu: recover hung GPU!&lt;/SPAN&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;However we were able to resolve the issue and now its running smooth with the weston and sway compositor with 4GiB RAM usage.&lt;BR /&gt;&lt;BR /&gt;As this was done for the customer we are unable to share the details, in case of support please reach-out to us on &lt;A href="mailto:rutvij.trivedi@siliconsignals.io" target="_blank" rel="noopener"&gt;rutvij.trivedi@siliconsignals.io&lt;/A&gt; or visit &lt;A href="http://www.siliconsignals.io" target="_blank" rel="noopener"&gt;www.siliconsignals.io&lt;/A&gt;.&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;BR&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 14:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-driver-crash-on-i-MX8M-Mini-with-4GB-RAM/m-p/1729012#M213115</guid>
      <dc:creator>r_trivedi123</dc:creator>
      <dc:date>2023-09-25T14:35:47Z</dc:date>
    </item>
  </channel>
</rss>