<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFreeRTOS tick on ImX8</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907838#M136838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it correct saying that FreeRTOS port for Imx8 - m4 core does not support scheduler evaluation frequency higher than 1kHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 May 2019 16:00:21 GMT</pubDate>
    <dc:creator>luca_corna</dc:creator>
    <dc:date>2019-05-10T16:00:21Z</dc:date>
    <item>
      <title>FreeRTOS tick on ImX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907838#M136838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it correct saying that FreeRTOS port for Imx8 - m4 core does not support scheduler evaluation frequency higher than 1kHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 16:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907838#M136838</guid>
      <dc:creator>luca_corna</dc:creator>
      <dc:date>2019-05-10T16:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS tick on ImX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907839#M136839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;By default, the maximum FreeRTOS tick rate is 1 kHz (1 ms). But you can go to a higher frequency. For this you have to provide your own version of the pdMS_TO_TICKS() macro in FreeRTOSconfig.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 06:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907839#M136839</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-05-13T06:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS tick on ImX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907840#M136840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So if I want that the scheduler re-evaluate every 100us I have simply to&amp;nbsp; add:&lt;/P&gt;&lt;P&gt;#define configTICK_RATE_HZ 10000&lt;/P&gt;&lt;P&gt;#define pdMS_TO_TICK ( timeInUs ) ( timeInUs *&amp;nbsp;&lt;SPAN&gt;configTICK_RATE_HZ&amp;nbsp;&lt;/SPAN&gt; /1000000 )&lt;/P&gt;&lt;P&gt;right? in this case ms_to_tick is actually us_to_tick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 09:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907840#M136840</guid>
      <dc:creator>luca_corna</dc:creator>
      <dc:date>2019-05-13T09:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS tick on ImX8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907841#M136841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Older FreeRTOS ports used something like this:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="token function"&gt;vTaskDelay&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;50&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;portTICK_RATE_MS&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;Which is a problem if the tick rate &amp;gt;1 kHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's why newer FreeRTOS ports (I think from 9.0.0 on) use the pdMS_TO_TICKS() macro:&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;vTaskDelay(pdMS_TO_TICKS(50));&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;which is defined as&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="comment token"&gt;/* Converts a time in milliseconds to a time in ticks.  This macro can be
overridden by a macro of the same name defined in FreeRTOSConfig.h in case the
definition here is not suitable for your application. */&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#ifndef pdMS_TO_TICKS&lt;/SPAN&gt;
 &lt;SPAN class="property macro token"&gt;#define pdMS_TO_TICKS( xTimeInMs ) ( ( TickType_t ) ( ( ( TickType_t ) ( xTimeInMs ) * ( TickType_t ) configTICK_RATE_HZ ) / ( TickType_t ) 1000 ) )&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#endif&lt;/SPAN&gt;
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;in projdefs.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So as long as you are using pdMS_TO_TICKS and not portTICK_RATE_MS you are fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 10:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FreeRTOS-tick-on-ImX8/m-p/907841#M136841</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-05-13T10:50:51Z</dc:date>
    </item>
  </channel>
</rss>