<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MQ M4 UART problem.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-M4-UART-problem/m-p/907127#M136780</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I’m afraid that TechNexion boards are not supported by NXP. You could redirect your question directly to TechNexion on the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.technexion.com/support/"&gt;https://www.technexion.com/support/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 May 2019 16:31:35 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2019-05-29T16:31:35Z</dc:date>
    <item>
      <title>IMX8MQ M4 UART problem.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-M4-UART-problem/m-p/907126#M136779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a IMX8MQ eval board from TechNexion, while playing around with the M4 Core of the SOC I noticed that in all examples provided I am not able to recieve using UART but am able to transmit without a problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the SDK provided by them (SDK version 2.3)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried all UART recieve APIs but all in vain.&lt;/P&gt;&lt;P&gt;I checked the device tree files so as to make sure that the device tree initialization is not conflicting with what I have defined for M4 Core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/TechNexion/freertos-tn/tree/freertos_SDK_2.3_IMX8M/boards/pico-8m-m4/demo_apps/hello_world"&gt;Link to the project &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I even checked the hardware the UART singals are there till the SOC Pins.&lt;/P&gt;&lt;P&gt;I also tried changing ports but still no luck..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated..!!&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2019 08:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-M4-UART-problem/m-p/907126#M136779</guid>
      <dc:creator>siva3</dc:creator>
      <dc:date>2019-05-24T08:52:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ M4 UART problem.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-M4-UART-problem/m-p/907127#M136780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I’m afraid that TechNexion boards are not supported by NXP. You could redirect your question directly to TechNexion on the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.technexion.com/support/"&gt;https://www.technexion.com/support/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 16:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-M4-UART-problem/m-p/907127#M136780</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-05-29T16:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ M4 UART problem.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-M4-UART-problem/m-p/907128#M136781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem was solved, the pin mux definitions was wrong, fixing it fixed the issue,, :smileyhappy:&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jun 2019 08:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-M4-UART-problem/m-p/907128#M136781</guid>
      <dc:creator>siva3</dc:creator>
      <dc:date>2019-06-15T08:06:41Z</dc:date>
    </item>
  </channel>
</rss>