<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Dual OpenGL application v-sync issue on i.MX6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906770#M136755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! I'll check the driver in the BSP version you mentioned.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 May 2019 05:21:30 GMT</pubDate>
    <dc:creator>frankchenmh</dc:creator>
    <dc:date>2019-05-30T05:21:30Z</dc:date>
    <item>
      <title>Dual OpenGL application v-sync issue on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906766#M136751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, we got an issue about i.MX6 dual OpenGL applications (render to two framebuffers).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer board based on i.MX6Q sabresd.&lt;BR /&gt;Linux BSP&lt;BR /&gt;GPU driver and sdk: L3.0.35_4.0.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fb0: PAL TVout, refresh rate 50Hz&lt;BR /&gt;fb2: HDMI, refresh rate 60Hz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OpenGL app1: render to fb0&lt;BR /&gt;OpenGL app2: render to fb2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The OpenGL applications are developed based on the samples in gpu_sdk_v1.00.tar.gz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the OpenGL applications render frames, the frames are synced with framebuffer v-sync. So the applications can run at the framerate same to the framebuffer refresh rate. When run app1 only, we can see that the app1 frame rate is 50Hz. When run app2 only, we can see the app2 frame rate is 60Hz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However if we run both app1 and app2, the framerate of app1 and app2 are both 50Hz no matter which app is started first. The app2 is synced with fb0 but not fb2. This is incorrect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example:&lt;BR /&gt;Step 1) Run app2. And we can see the frame rate of app2 is 60Hz.&lt;BR /&gt;Step 2) Run app1. Now the frame rate of app2 changes to 50Hz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help on how to fix this issue. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2019 10:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906766#M136751</guid>
      <dc:creator>frankchenmh</dc:creator>
      <dc:date>2019-05-24T10:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: Dual OpenGL application v-sync issue on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906767#M136752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is fixed on the new driver of the GPU you need to upgrade since we have not porting this driver to L3.0.35.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 14:57:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906767#M136752</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-05-28T14:57:36Z</dc:date>
    </item>
    <item>
      <title>Re: Dual OpenGL application v-sync issue on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906768#M136753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From which version of the BSP the GPU driver was updated to fix the issue? I'll check if it can be back ported to the BSP that I used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is there any standalone patch for this fix?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 15:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906768#M136753</guid>
      <dc:creator>frankchenmh</dc:creator>
      <dc:date>2019-05-28T15:13:52Z</dc:date>
    </item>
    <item>
      <title>Re: Dual OpenGL application v-sync issue on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906769#M136754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The fixed appear in L4.9.88 BSP version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 14:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906769#M136754</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-05-29T14:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: Dual OpenGL application v-sync issue on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906770#M136755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! I'll check the driver in the BSP version you mentioned.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 May 2019 05:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-OpenGL-application-v-sync-issue-on-i-MX6Q/m-p/906770#M136755</guid>
      <dc:creator>frankchenmh</dc:creator>
      <dc:date>2019-05-30T05:21:30Z</dc:date>
    </item>
  </channel>
</rss>