<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: CAN Bus: EMI capacitor values</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Bus-EMI-capacitor-values/m-p/905417#M136613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for considerations regarding capacitors selection one can look at AH1014&amp;nbsp; Fig.45&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/supporting-information/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf" title="https://www.nxp.com/docs/en/supporting-information/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf"&gt;https://www.nxp.com/docs/en/supporting-information/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2019 00:08:31 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-05-28T00:08:31Z</dc:date>
    <item>
      <title>CAN Bus: EMI capacitor values</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Bus-EMI-capacitor-values/m-p/905416#M136612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;BR /&gt;Using 3 of the TJA1042 CAN transceivers for a new design in conjunction with a i.MX8. The project managers have requested that the 3 channels be capable of 1Mbps each, with a default of 250kbps. I have all the circuits designed except for the EMI capacitor values. These are 2 matched capacitors in the pF range between CANH and GND, and CANL and GND.&lt;BR /&gt;From what I can find, the value of these will change depending on the bps. Given they want the potential full 1Mbps available for use, I assume I use the value suitable for this. I am struggling to find documentation on how to calculate the values though. I think it is around 35pF from a couple examples I have found. The TVS I am using has a Cd of 25-30pF so if this is the case, I may not need the capacitors at all.&lt;BR /&gt;Any links to a resource which shows how to calculate these values based on the kbps?&lt;BR /&gt;Thanks&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2019 02:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-Bus-EMI-capacitor-values/m-p/905416#M136612</guid>
      <dc:creator>pbain</dc:creator>
      <dc:date>2019-05-24T02:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Bus: EMI capacitor values</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Bus-EMI-capacitor-values/m-p/905417#M136613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for considerations regarding capacitors selection one can look at AH1014&amp;nbsp; Fig.45&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/supporting-information/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf" title="https://www.nxp.com/docs/en/supporting-information/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf"&gt;https://www.nxp.com/docs/en/supporting-information/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 00:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-Bus-EMI-capacitor-values/m-p/905417#M136613</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-28T00:08:31Z</dc:date>
    </item>
  </channel>
</rss>