<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX8QXP ISI input source in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/904869#M136518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;• Supported Pixel Formats when storing image into memory&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;below image format is only output format or both output and input format?&lt;/P&gt;&lt;P&gt;Pls&amp;nbsp;give detail reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Apr 2019 03:57:13 GMT</pubDate>
    <dc:creator>xu_ji1</dc:creator>
    <dc:date>2019-04-25T03:57:13Z</dc:date>
    <item>
      <title>I.MX8QXP ISI input source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/904867#M136516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question,If the camera sensor output image format is RAW,does I.MX8QXP ISI support the RAW image and processing it to YUV image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 07:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/904867#M136516</guid>
      <dc:creator>xu_ji1</dc:creator>
      <dc:date>2019-04-23T07:14:12Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8QXP ISI input source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/904868#M136517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;refer to the imx8x reference manual:&lt;/P&gt;&lt;P&gt;tream Manipulation Features&lt;BR /&gt;• Supported Pixel Formats when storing image into memory&lt;BR /&gt;• RAW8, RAW10, RAW12, RAW16&lt;BR /&gt;• RGB888, BGR888, RGB565, RGB 10-bit, BGR 10-bit&lt;BR /&gt;• YUV444, YUV422, YUV420 (8-bit, 10-bit, 12-bit)&lt;BR /&gt;• Plus more formats listed in the description of FORMAT field in the&lt;BR /&gt;channel's IMG_CTRL register&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Apr 2019 03:35:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/904868#M136517</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-04-25T03:35:22Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8QXP ISI input source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/904869#M136518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;• Supported Pixel Formats when storing image into memory&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;below image format is only output format or both output and input format?&lt;/P&gt;&lt;P&gt;Pls&amp;nbsp;give detail reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Apr 2019 03:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/904869#M136518</guid>
      <dc:creator>xu_ji1</dc:creator>
      <dc:date>2019-04-25T03:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8QXP ISI input source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/1450182#M189777</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The IMX8MPRM&amp;nbsp; ISI about P5267 says:&lt;/P&gt;&lt;P&gt;"• Input source will be converted to and processed by the processing pipeline&lt;BR /&gt;as YUV444 or RGB."&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;So what Input source are supported?&amp;nbsp; &amp;nbsp;Does&amp;nbsp; the camera sensor input&amp;nbsp; over MIPI have to be certain formats?&lt;/P&gt;&lt;P&gt;I saw the CAPTURE driver queries Sensor driver and convert the format by the following code:&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Pixel link input format&lt;BR /&gt;*/&lt;BR /&gt;struct mxc_isi_fmt mxc_isi_src_formats[] = {&lt;BR /&gt;{&lt;BR /&gt;.name = "RGB32",&lt;BR /&gt;.fourcc = V4L2_PIX_FMT_RGB32,&lt;BR /&gt;.depth = { 32 },&lt;BR /&gt;.memplanes = 1,&lt;BR /&gt;.colplanes = 1,&lt;BR /&gt;}, {&lt;BR /&gt;.name = "YUV32 (X-Y-U-V)",&lt;BR /&gt;.fourcc = V4L2_PIX_FMT_YUV32,&lt;BR /&gt;.depth = { 32 },&lt;BR /&gt;.memplanes = 1,&lt;BR /&gt;.colplanes = 1,&lt;BR /&gt;}&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;struct mxc_isi_fmt *mxc_isi_get_src_fmt(struct v4l2_subdev_format *sd_fmt)&lt;BR /&gt;{&lt;BR /&gt;u32 index;&lt;/P&gt;&lt;P&gt;/* two fmt RGB32 and YUV444 from pixellink */&lt;BR /&gt;if (sd_fmt-&amp;gt;format.code == MEDIA_BUS_FMT_YUYV8_1X16 ||&lt;BR /&gt;sd_fmt-&amp;gt;format.code == MEDIA_BUS_FMT_YVYU8_2X8 ||&lt;BR /&gt;sd_fmt-&amp;gt;format.code == MEDIA_BUS_FMT_AYUV8_1X32 ||&lt;BR /&gt;sd_fmt-&amp;gt;format.code == MEDIA_BUS_FMT_UYVY8_2X8 ||&lt;BR /&gt;sd_fmt-&amp;gt;format.code == MEDIA_BUS_FMT_YUYV8_2X8)&lt;BR /&gt;index = 1;&lt;BR /&gt;else&lt;BR /&gt;index = 0;&lt;BR /&gt;return &amp;amp;mxc_isi_src_formats[index];&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;But our AR0234 uses&amp;nbsp;MEDIA_BUS_FMT_SBGGR8_1X8,&amp;nbsp; the output image is duplicated and half height as the attached picture. And the width and height were set correctly in the register,&amp;nbsp; Any suggestion?&lt;/P&gt;&lt;P&gt;We can provide more information and trace upon request.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="test31A.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/178230i32C8D75BD4C5F863/image-size/large?v=v2&amp;amp;px=999" role="button" title="test31A.jpg" alt="test31A.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;test31A.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tony&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 22:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8QXP-ISI-input-source/m-p/1450182#M189777</guid>
      <dc:creator>PLIU168</dc:creator>
      <dc:date>2022-04-27T22:19:41Z</dc:date>
    </item>
  </channel>
</rss>