<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRecovery time from SUSPEND and WAIt modes</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Recovery-time-from-SUSPEND-and-WAIt-modes/m-p/216164#M13649</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX5x PM driver supports different modes of low power operations.&lt;/P&gt;&lt;P&gt;I'm particularly interested in the:&lt;/P&gt;&lt;P&gt;- STOP mode which maps to "Suspend to RAM"&lt;/P&gt;&lt;P&gt;- WAIT mode which maps to "Standby" mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know what is the recovery time needed from the low poer modes listed above to full running mode ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our idea is to read an ADC value each 1s. If the value is below a certain threshold we get back to WAIT (or STOP mode depending of the staus of the external PSU) mode. Are such fast (1 second) transition times even possible ? Looking at the source there should be no limitations, except for some PLL setup times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts, comments ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2012 22:04:53 GMT</pubDate>
    <dc:creator>MarkoPanger</dc:creator>
    <dc:date>2012-03-01T22:04:53Z</dc:date>
    <item>
      <title>Recovery time from SUSPEND and WAIt modes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recovery-time-from-SUSPEND-and-WAIt-modes/m-p/216164#M13649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX5x PM driver supports different modes of low power operations.&lt;/P&gt;&lt;P&gt;I'm particularly interested in the:&lt;/P&gt;&lt;P&gt;- STOP mode which maps to "Suspend to RAM"&lt;/P&gt;&lt;P&gt;- WAIT mode which maps to "Standby" mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know what is the recovery time needed from the low poer modes listed above to full running mode ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our idea is to read an ADC value each 1s. If the value is below a certain threshold we get back to WAIT (or STOP mode depending of the staus of the external PSU) mode. Are such fast (1 second) transition times even possible ? Looking at the source there should be no limitations, except for some PLL setup times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts, comments ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2012 22:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recovery-time-from-SUSPEND-and-WAIt-modes/m-p/216164#M13649</guid>
      <dc:creator>MarkoPanger</dc:creator>
      <dc:date>2012-03-01T22:04:53Z</dc:date>
    </item>
  </channel>
</rss>