<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Custom Data Saving in eFuse  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Data-Saving-in-eFuse/m-p/904303#M136447</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. Is there have other register can be used to save custom data and will not have any effect?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. No, the OCOTP_GPx fuse words are the only ones that can be used for general purpose software tasks without any side effect.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 May 2019 12:11:42 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2019-05-13T12:11:42Z</dc:date>
    <item>
      <title>Custom Data Saving in eFuse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Data-Saving-in-eFuse/m-p/904302#M136446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I want to save some custom data into eFuse. After reading the iMX7 - Reference Manual, I think "OCOTP_GP" can be used and will not affect the operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the&amp;nbsp;size of that register is not enough. Is there have&amp;nbsp;other register can be used to save custom data and will not have any effect?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jacky&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 01:32:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-Data-Saving-in-eFuse/m-p/904302#M136446</guid>
      <dc:creator>jacky_cheng</dc:creator>
      <dc:date>2019-05-08T01:32:13Z</dc:date>
    </item>
    <item>
      <title>Re: Custom Data Saving in eFuse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-Data-Saving-in-eFuse/m-p/904303#M136447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. Is there have other register can be used to save custom data and will not have any effect?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. No, the OCOTP_GPx fuse words are the only ones that can be used for general purpose software tasks without any side effect.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 12:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-Data-Saving-in-eFuse/m-p/904303#M136447</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-05-13T12:11:42Z</dc:date>
    </item>
  </channel>
</rss>