<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: 4 camera capturing via MIPI-CSI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/4-camera-capturing-via-MIPI-CSI/m-p/903891#M136375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jimmychan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate your support. I got it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Apr 2019 09:09:44 GMT</pubDate>
    <dc:creator>Kazuma_Sasaki</dc:creator>
    <dc:date>2019-04-24T09:09:44Z</dc:date>
    <item>
      <title>4 camera capturing via MIPI-CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-camera-capturing-via-MIPI-CSI/m-p/903889#M136373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are under considering surround view system with i.MX6 Solo. Please let me clarify supporting number of cameras.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we connect camera via MIPI-CSI interface, we are using virtual channels feature.&lt;/P&gt;&lt;P&gt;I think each virtual channel binding to IPU-CSIn port. then, i.MX6Solo only have two CSI port.&lt;/P&gt;&lt;P&gt;I suppose i.MX6 Solo is able to capture simulateously up to 2 cameras,&lt;/P&gt;&lt;P&gt;But, i.MX6SDL reference manual says "MIPI CSI supports up to 4 virtual channel".&lt;/P&gt;&lt;P&gt;Can i.MX6 Solo use four virtual channels simulateously?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found following thread regarding same topics.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/353930"&gt;The meaning of i.MX6 MIPI-CSI "virtual channel".&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If iMX6 Solo is able to connect 4 cameras via virtual channels of MIPI-CSI,&lt;/P&gt;&lt;P&gt;How do I configure the GPR13 register? should I change port mapping by each frames?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2019 12:33:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-camera-capturing-via-MIPI-CSI/m-p/903889#M136373</guid>
      <dc:creator>Kazuma_Sasaki</dc:creator>
      <dc:date>2019-04-22T12:33:41Z</dc:date>
    </item>
    <item>
      <title>Re: 4 camera capturing via MIPI-CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-camera-capturing-via-MIPI-CSI/m-p/903890#M136374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is only 1 IPU in i.MX6S. It is not able to handle 4 cameras signals.&lt;/P&gt;&lt;P&gt;Even i.MX6Q, it is needed a FPGA in between cameras and i.MX6.&lt;/P&gt;&lt;P&gt;For your reference, this discussed in &lt;A href="https://community.nxp.com/thread/301812"&gt;4 video capture using MIPI-CSI2 port&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, we have a solution for surround view that using PCIe.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95143"&gt;iMX6 TW686x Surround view patch&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you may consider using i.MX8.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/nxp-designs/surround-view-application:SURROUND-VIEW-APPLICATION" title="https://www.nxp.com/support/developer-resources/nxp-designs/surround-view-application:SURROUND-VIEW-APPLICATION"&gt;Surround View Application | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 07:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-camera-capturing-via-MIPI-CSI/m-p/903890#M136374</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2019-04-24T07:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: 4 camera capturing via MIPI-CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/4-camera-capturing-via-MIPI-CSI/m-p/903891#M136375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jimmychan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate your support. I got it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 09:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/4-camera-capturing-via-MIPI-CSI/m-p/903891#M136375</guid>
      <dc:creator>Kazuma_Sasaki</dc:creator>
      <dc:date>2019-04-24T09:09:44Z</dc:date>
    </item>
  </channel>
</rss>