<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDrive strength setting for CSI Port1</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Drive-strength-setting-for-CSI-Port1/m-p/903780#M136344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;3&lt;/P&gt;&lt;P&gt;We have designed one custom board based on iMX8M SOC.In this we are using camera(OV5640) mezzanine from D3 engineering.We are planning pre-compliance testing for this custom board and observed that CSI port1 differential clock is radiating.For termination settings of this clcok we are following IMX8MDQLQRM reference manual Rev. 1, 04/2019. and we found that there is no General Purpose Register information for CSI1 port.This detailed information is given for CSI2 port(Section 8.2.4.35 GPR34 General Purpose Register (IOMUXC_GPR_GPR34) ).Is there any way/Document to change termination value of CSI1 port?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sandeep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 May 2019 13:25:16 GMT</pubDate>
    <dc:creator>sandeep_yenugul</dc:creator>
    <dc:date>2019-05-07T13:25:16Z</dc:date>
    <item>
      <title>Drive strength setting for CSI Port1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Drive-strength-setting-for-CSI-Port1/m-p/903780#M136344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;3&lt;/P&gt;&lt;P&gt;We have designed one custom board based on iMX8M SOC.In this we are using camera(OV5640) mezzanine from D3 engineering.We are planning pre-compliance testing for this custom board and observed that CSI port1 differential clock is radiating.For termination settings of this clcok we are following IMX8MDQLQRM reference manual Rev. 1, 04/2019. and we found that there is no General Purpose Register information for CSI1 port.This detailed information is given for CSI2 port(Section 8.2.4.35 GPR34 General Purpose Register (IOMUXC_GPR_GPR34) ).Is there any way/Document to change termination value of CSI1 port?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sandeep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2019 13:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Drive-strength-setting-for-CSI-Port1/m-p/903780#M136344</guid>
      <dc:creator>sandeep_yenugul</dc:creator>
      <dc:date>2019-05-07T13:25:16Z</dc:date>
    </item>
    <item>
      <title>Re: Drive strength setting for CSI Port1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Drive-strength-setting-for-CSI-Port1/m-p/903781#M136345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sandeep&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there is no "CSI1 port", there are two MIPI CSI2 ports :&lt;/P&gt;&lt;P&gt;section 8.2.4.35 gives description of CSI2_1_RX_RCAL&lt;/P&gt;&lt;P&gt;CSI2_2_RX_RCAL is described in sect.8.2.4.42 GPR41 General Purpose Register (IOMUXC_GPR_GPR41)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 00:06:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Drive-strength-setting-for-CSI-Port1/m-p/903781#M136345</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-08T00:06:54Z</dc:date>
    </item>
  </channel>
</rss>