<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:     iMX8QM SCU DDR Configuration Issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-SCU-DDR-Configuration-Issue/m-p/903135#M136272</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are waiting for your valuable reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashanth Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 May 2019 04:51:21 GMT</pubDate>
    <dc:creator>prashanthkumar</dc:creator>
    <dc:date>2019-05-10T04:51:21Z</dc:date>
    <item>
      <title>iMX8QM SCU DDR Configuration Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-SCU-DDR-Configuration-Issue/m-p/903134#M136271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on iMX8QM Custom board with 4.14.98 Kernel BSP (1.2 SCU Firmware). We have boards with 2GB, 4GB &amp;amp; 6GB DDR configuration. By default only one of the DDR configuration will support while compilation time.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The SCFW Compilation Command: &lt;BR /&gt;make qm R=B0 B=val M=1 DDR_CON=dcd_b0_6GB_1.6GHz U=2&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But we need to compile multiple DDR files, output should be single "scfw_tcm.bin" binary &amp;amp; should support different boards having different DDR configuration. We have some board configuration GPIOs, which is having hardware pull up. Is it possible to differentiate &amp;amp; initialize/compile different DDR configuration (2GB/4Gb/6GB) files based on these board configuration GPIOs in SCFW?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashanth Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2019 10:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-SCU-DDR-Configuration-Issue/m-p/903134#M136271</guid>
      <dc:creator>prashanthkumar</dc:creator>
      <dc:date>2019-05-07T10:09:27Z</dc:date>
    </item>
    <item>
      <title>Re:     iMX8QM SCU DDR Configuration Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-SCU-DDR-Configuration-Issue/m-p/903135#M136272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are waiting for your valuable reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Prashanth Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 04:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-SCU-DDR-Configuration-Issue/m-p/903135#M136272</guid>
      <dc:creator>prashanthkumar</dc:creator>
      <dc:date>2019-05-10T04:51:21Z</dc:date>
    </item>
    <item>
      <title>Re:     iMX8QM SCU DDR Configuration Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-SCU-DDR-Configuration-Issue/m-p/903136#M136273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the current SCU firmware implementation, there is no way to dynamically configure the DDR parameters depending on any conditions during the ROM and SCFW boot flow.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 09:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-SCU-DDR-Configuration-Issue/m-p/903136#M136273</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-05-13T09:29:31Z</dc:date>
    </item>
  </channel>
</rss>