<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックProfiler for iMX23 evk running Linux...</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Profiler-for-iMX23-evk-running-Linux/m-p/215946#M13623</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using iMX23 evk which is running Linux 2.6.31(downloaded from freescale site).&lt;/P&gt;&lt;P&gt;I have developed one application that is running on the kit.&lt;/P&gt;&lt;P&gt;I want to profile that application. I know there are some profilers like gprof which can be used to profile application in linux environment. but i am not sure whether it works for this Linux provided by freescale. can anyone tell me whether i can use any profiler with the iMX23 evk? if yes then which profiler? and how i can add that profiler to my kernel image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Feb 2012 04:07:07 GMT</pubDate>
    <dc:creator>KartikDetroja</dc:creator>
    <dc:date>2012-02-29T04:07:07Z</dc:date>
    <item>
      <title>Profiler for iMX23 evk running Linux...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Profiler-for-iMX23-evk-running-Linux/m-p/215946#M13623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using iMX23 evk which is running Linux 2.6.31(downloaded from freescale site).&lt;/P&gt;&lt;P&gt;I have developed one application that is running on the kit.&lt;/P&gt;&lt;P&gt;I want to profile that application. I know there are some profilers like gprof which can be used to profile application in linux environment. but i am not sure whether it works for this Linux provided by freescale. can anyone tell me whether i can use any profiler with the iMX23 evk? if yes then which profiler? and how i can add that profiler to my kernel image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Feb 2012 04:07:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Profiler-for-iMX23-evk-running-Linux/m-p/215946#M13623</guid>
      <dc:creator>KartikDetroja</dc:creator>
      <dc:date>2012-02-29T04:07:07Z</dc:date>
    </item>
  </channel>
</rss>