<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx6 Aptina AR0330 MIPI interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901847#M136038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;why don't you set it output rgb656 which imx6 supports it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 May 2019 08:24:38 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2019-05-08T08:24:38Z</dc:date>
    <item>
      <title>i.mx6 Aptina AR0330 MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901844#M136035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to interface MIPI camera-ar0330&amp;nbsp; with imx6 duallite processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.kailaptech.com/Product.aspx?id=1271&amp;amp;l1=1269" target="test_blank"&gt;http://www.kailaptech.com/Product.aspx?id=1271&amp;amp;l1=1269&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;As ar0330 is image sensor, Is it another DSP required between imx6 &amp;amp; ar0330 to convert row data to video mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Camera interface is new for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Jignesh Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 May 2019 05:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901844#M136035</guid>
      <dc:creator>jigneshpatel</dc:creator>
      <dc:date>2019-05-06T05:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Aptina AR0330 MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901845#M136036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;imx6q has mipi csi interface, can support this camera, you don't need dsp to convert, for the driver, you can refer to the “/drivers/media/video/mxc/capture/ov5640_mipi.c", to change the source code based on your own mipi camera&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 07:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901845#M136036</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-05-08T07:10:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Aptina AR0330 MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901846#M136037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Joan Xie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As my understanding, ar0330 has output format raw bayer pattern and imx6 doesn'y support it.&lt;/P&gt;&lt;P&gt;Imx6's IC is not able to convert raw bayer pattern to YUV422(supported by imx6).&lt;/P&gt;&lt;P&gt;So to get YUV422 formate on video input of imx6,&amp;nbsp; Is it required to ISP for raw data formatter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me correct if i am wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jignesh Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 07:35:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901846#M136037</guid>
      <dc:creator>jigneshpatel</dc:creator>
      <dc:date>2019-05-08T07:35:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Aptina AR0330 MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901847#M136038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;why don't you set it output rgb656 which imx6 supports it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 08:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901847#M136038</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-05-08T08:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Aptina AR0330 MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901848#M136039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Joan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it rgb656 or rgb565?&lt;/P&gt;&lt;P&gt;I am doing camera integration first time so have some confusion about the raw data format of camera.&lt;/P&gt;&lt;P&gt;1. ar0330 output format is output is bayer pattern( 12 to 10-bit output A-law compression), Is it same rgb656 or I need to convert raw data to rgb656 in software? &lt;/P&gt;&lt;P&gt;2. Will I get same quality of&amp;nbsp; image/video, if i imx6 successfully integret directly with ar0330(without ISP).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for helping me for improve understanding of camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jignesh Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 09:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901848#M136039</guid>
      <dc:creator>jigneshpatel</dc:creator>
      <dc:date>2019-05-08T09:45:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Aptina AR0330 MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901849#M136040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have ar0330&amp;nbsp; data sheet, you can refer to that, I think ar0330&amp;nbsp; can output many formats, not only bayer pattern, you can choose one format imx6 csi can support, then you don't need any converter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 May 2019 01:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Aptina-AR0330-MIPI-interface/m-p/901849#M136040</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-05-09T01:56:22Z</dc:date>
    </item>
  </channel>
</rss>