<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Booting error in imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-error-in-imx6/m-p/900745#M135928</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thakns for response, yes I could fix It. I updated all system, bootloader, kernel and rootfs and It works.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 May 2019 11:30:45 GMT</pubDate>
    <dc:creator>emmanuelperea</dc:creator>
    <dc:date>2019-05-06T11:30:45Z</dc:date>
    <item>
      <title>Booting error in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-error-in-imx6/m-p/900743#M135926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working with imx6 dual lite conncectore of digi. I am using a 4.9 kernel builfing with yocto 2.4. It was working fine, I have some issues with display but i could boot and operative system init. Until I made a mistake, I mounted mmcblk0p3 i a folder and I replaced the etc folder with another etc folder that I copied flrom another imx6 board, but before that the second etc folder I copied in a windows system. Plus I umounted and mounted the mmcblk0p1 in /mnt/linux to change a dtb file. After that I restart the board but dont start again I had this uotuputs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities&lt;BR /&gt;EXT4-fs (mmcblk0p3): couldn't mount as ext2 due to feature incompatibilities&lt;BR /&gt;EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;VFS: Mounted root (ext4 filesystem) on device 179:3.&lt;BR /&gt;devtmpfs: mounted&lt;BR /&gt;Freeing unused kernel memory: 1024K&lt;BR /&gt;Starting init: /sbin/init exists but couldn't execute it (error -14)&lt;BR /&gt;Starting init: /bin/sh exists but couldn't execute it (error -14)&lt;BR /&gt;Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidanc.&lt;BR /&gt;CPU0: stopping&lt;BR /&gt;CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.9.81-dey+g2c6ae4c #2&lt;BR /&gt;Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---[ end Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt fo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading this I think that kernel is initialized and mmcblk0p3 ext4 is monted, but there is an init error for some reason. I tried to boot from tftp but I had the same problem, and I updated kernel and rootfs in the board but I had the same problem.&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 May 2019 13:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-error-in-imx6/m-p/900743#M135926</guid>
      <dc:creator>emmanuelperea</dc:creator>
      <dc:date>2019-05-04T13:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: Booting error in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-error-in-imx6/m-p/900744#M135927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Emmanuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to reflash images :&lt;BR /&gt;&lt;A class="link-titled" href="https://www.digi.com/products/embedded-systems/system-on-modules/connectcore-imx6#productsupport" title="https://www.digi.com/products/embedded-systems/system-on-modules/connectcore-imx6#productsupport"&gt;https://www.digi.com/products/embedded-systems/system-on-modules/connectcore-imx6#productsupport&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;also issue may be posted on digi forum&lt;BR /&gt;&lt;A class="link-titled" href="https://www.digi.com/support/forum/" title="https://www.digi.com/support/forum/"&gt;Digi Forum&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 May 2019 22:53:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-error-in-imx6/m-p/900744#M135927</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-05T22:53:43Z</dc:date>
    </item>
    <item>
      <title>Re: Booting error in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-error-in-imx6/m-p/900745#M135928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thakns for response, yes I could fix It. I updated all system, bootloader, kernel and rootfs and It works.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 May 2019 11:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-error-in-imx6/m-p/900745#M135928</guid>
      <dc:creator>emmanuelperea</dc:creator>
      <dc:date>2019-05-06T11:30:45Z</dc:date>
    </item>
  </channel>
</rss>