<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Decoding multiple H.264 streams with i.MX8M VPU? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900532#M135912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response, but I guess my question was not clear enough, so let me get more specific:&lt;/P&gt;&lt;P&gt;My customer is using several IP cameras and their capture should be shown on a display. So there are 2-4 H.264 streams that have to be decoded.&lt;/P&gt;&lt;P&gt;Is this possible with the i.MX8M VPU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 May 2019 06:05:58 GMT</pubDate>
    <dc:creator>martin_gisbert</dc:creator>
    <dc:date>2019-05-23T06:05:58Z</dc:date>
    <item>
      <title>Decoding multiple H.264 streams with i.MX8M VPU?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900530#M135910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the i.MX8M's VPU features a 1080p60 H.264 decoder (up to high profile). Is it possible to use this VPU to decode *multiple* streams with a lower frame rate, e.g. 4 streams of 15 fps each? Or possibly even more streams with a lower resolution and/or profile, like maybe 6 x 720p15 (low profile)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 11:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900530#M135910</guid>
      <dc:creator>martin_gisbert</dc:creator>
      <dc:date>2019-05-20T11:01:05Z</dc:date>
    </item>
    <item>
      <title>Re: Decoding multiple H.264 streams with i.MX8M VPU?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900531#M135911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes its possible, MX8M its up to&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;4K @ 60fps with High Dynamic Range:&lt;/STRONG&gt;&lt;BR /&gt;- h.265&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;4K @ 30fps&lt;/STRONG&gt;&lt;BR /&gt;- h.264 &lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;A class="link-titled" href="https://imxdev.gitlab.io/tutorial/How_to_use_dual_display_on_i.MX8_including_4k_decoding/" title="https://imxdev.gitlab.io/tutorial/How_to_use_dual_display_on_i.MX8_including_4k_decoding/"&gt;How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2019 14:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900531#M135911</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-05-21T14:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: Decoding multiple H.264 streams with i.MX8M VPU?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900532#M135912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response, but I guess my question was not clear enough, so let me get more specific:&lt;/P&gt;&lt;P&gt;My customer is using several IP cameras and their capture should be shown on a display. So there are 2-4 H.264 streams that have to be decoded.&lt;/P&gt;&lt;P&gt;Is this possible with the i.MX8M VPU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 06:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900532#M135912</guid>
      <dc:creator>martin_gisbert</dc:creator>
      <dc:date>2019-05-23T06:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: Decoding multiple H.264 streams with i.MX8M VPU?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900533#M135913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got the same question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2to4 IP Streams from Camera and it should be shown on monitor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible with i.MX8M or i.MX8MQM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2020 14:38:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Decoding-multiple-H-264-streams-with-i-MX8M-VPU/m-p/900533#M135913</guid>
      <dc:creator>marcelbässler</dc:creator>
      <dc:date>2020-01-07T14:38:35Z</dc:date>
    </item>
  </channel>
</rss>