<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900252#M135874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more thing:&lt;/P&gt;&lt;P&gt;From a cost-perspective, DDR3L and DDR4 components are a lot cheaper "per Gigabit of Memory" than LPDDR4. Given todays market prices, LPDDR4 is almost twice as expensive than DDR3L or DDR4 for the same amount of memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But DDR3L and DDR4 components are only available in a x8 or x16 configuration, requiring to use multiple components to fill the bus-width of a rank. If you use a 32 bit wide bus, you would need to connect four pieces of x8 or two pieces of x16 components to each rank (with LPDDR4 you could just have one chip and you're done!).&lt;/P&gt;&lt;P&gt;Note: The i.MX8 supports maximum two ranks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both DDR4 and LPDDR4 are technologies which are limited to the worlds largest DRAM manufacturers. These big manufacturers require customers taking hundreds of millions of parts from them to fill their fab. Surely 99% or maybe more of the output of DDR4 and LPDDR4 goes into PC's, laptops, smartphones and tablets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now think about the following:&lt;/P&gt;&lt;P&gt;In latest a year all these applications will have changed to DDR5 and LPDDR5. The demand for DDR4 and LPDDR4 then might drop to only 1% of industrial customers. What do you think will the biggest manufacturers do? Will they continue making DDR4 and LPDDR4 ? I have doubts!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the past, with all former memory technologies, smaller "fabless" DRAM makers jumped on the technology and produced compatible alternative parts. But the bad news is: This door is almost closed as the production of high-capacity DDR4 and LPDDR4 components requires production-technologies of 20nm or smaller, which cost BILLIONS of dollars. Only the largest memory-firms can afford that. Eventually the one or another fabless company will simply buy the parts from the big companies and marks them with their own part number, but once the large manufacturer goes EOL, the product from the smaller company will die as well, as it is the same chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might only see some lower-density DDR4 and LPDDR4 from other fabless manufacturers which offer longevity. I know that Intelligent Memory has designed some DDR4 and LPDDR4 "with on-chip ECC error-correction" (which increases system-availability and reliability a lot!), but I do not yet see any other companies with plans for such parts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While DDR3L technology sounds "outdated" to some people, it will be the technology that can securely survive long-term, simple because there are lots of manufacturers offering such parts and the demand for DDR3L does not depend on mass-market applications like computers, phones or tables.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Thorsten Wronski&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Memphis Electronic AG&lt;/P&gt;&lt;P&gt;We Know Memory&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.memphis.ag"&gt;www.memphis.ag&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jul 2019 12:52:50 GMT</pubDate>
    <dc:creator>twmemphis</dc:creator>
    <dc:date>2019-07-19T12:52:50Z</dc:date>
    <item>
      <title>iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900242#M135864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Is there a single chip LPDDR4 4GByte RAM chip that is compatible with the iMX8M-Mini processor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 May 2019 08:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900242#M135864</guid>
      <dc:creator>gap</dc:creator>
      <dc:date>2019-05-04T08:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900243#M135865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX 8M Mini supports x32/16 bit DRAM interfaces.&amp;nbsp;LPDDR4 is essentially dual channeled; using single channel means half of memory is lost. About the LDDR4 configure you can see the script here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-340179"&gt;i.MX8 MSCALE SERIES DDR Tool Release (V2.10)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 May 2019 06:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900243#M135865</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-05-05T06:24:31Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900244#M135866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Thanks for the info. I'm trying to decide which memory to use to design the iMX8M-Mini with 4GBytes RAM. I can only find x32 4GB parts that are QDP(&lt;SPAN style="font-size: 11.0pt;"&gt;quad die package) which the &lt;SPAN style="display: inline !important; float: none; background-color: transparent; color: #3d3d3d; font-family: Helvetica Neue,Helvetica,Arial,Lucida Grande,sans-serif; font-size: 15px; font-style: normal; font-variant: normal; font-weight: 400; letter-spacing: normal; orphans: 2; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px; word-wrap: break-word;"&gt; iMX8M-Mini&lt;/SPAN&gt; doesn't support. The largest DDP (dual die package) LPDDR4 i can find is 2GB. What RAM configuration would you suggest i use to get 4GB RAM please?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 May 2019 08:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900244#M135866</guid>
      <dc:creator>gap</dc:creator>
      <dc:date>2019-05-05T08:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900245#M135867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you checked MT53D1024M32xxx? It has the same datasheet with DDR4 used in the reference design. I guess i.mx8 mini has control pins for 4 GByte DDR4 which are shown as NC(not connected) in 2 GB DDR4 schematic page and connected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 13:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900245#M135867</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2019-05-16T13:17:29Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900246#M135868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, The iMX8M-Mini doesn't support QDP (Quad-Die, Dual-Channel, Dual-Rank Package) and the only 4GByte&amp;nbsp;parts including the one you have mentioned are QDP. In that same datasheet the 2Gbyte part is DDP (Dual-Die, Dual-Channel, Single-Rank Package). I think we are going to go with a single chip 2Gbyte part design and hope a DDP 4Gbyte part is available in the future. Thanks for your input.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 14:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900246#M135868</guid>
      <dc:creator>gap</dc:creator>
      <dc:date>2019-05-16T14:53:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900247#M135869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi Graeme,&lt;/P&gt;&lt;P&gt;Why do you think i.MX8M Mini doesn't support QDP ? We have successfully deployed Micron MT53D1024M32D4DT-053 on our i.MX8M Mini board.&lt;/P&gt;&lt;P&gt;Felix.&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 13:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900247#M135869</guid>
      <dc:creator>felixradensky</dc:creator>
      <dc:date>2019-06-28T13:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900248#M135870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;It came from one of the datasheets.&lt;/P&gt;&lt;P&gt;I've not been working on the iMX8M-mini for a few weeks but thanks for the info.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 13:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900248#M135870</guid>
      <dc:creator>gap</dc:creator>
      <dc:date>2019-06-28T13:32:57Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900249#M135871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;I've just found this is an old&amp;nbsp;email from one of our distributors, maybe he was wrong?&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;STRONG style="font-size: 11pt; "&gt;Please note that&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;STRONG style="color: #0070c0; font-size: 11pt; "&gt;MT53D1024M32D4DT-053 WT:D&lt;/STRONG&gt;&lt;SPAN style="font-size: 11pt;"&gt; – &lt;/SPAN&gt;&lt;SPAN style="font-size: 11pt;"&gt;200ball VFBGA &lt;/SPAN&gt;&lt;SPAN style="font-size: 11pt;"&gt;FBGA – DID Z11M &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN style="font-size: 11pt;"&gt;SDRAM 32Gb LPDDR4 1GX32 1.1V .- &lt;/SPAN&gt;&lt;SPAN style="font-size: 11pt;"&gt;1866 MHz – QDP&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;STRONG style="font-size: 11pt; "&gt;Is not supported&lt;/STRONG&gt;&lt;SPAN style="font-size: 11pt;"&gt; because i.MX 8M Mini does not support byte mode which is required for quad die package (QDP) dual channel dual rank &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN style="font-size: 11pt;"&gt;Supported (JESD209-4B ) is dual die dual channel single rank (=32bit) and single die single channel single rank (=16bit) with x16mode&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 14:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900249#M135871</guid>
      <dc:creator>gap</dc:creator>
      <dc:date>2019-06-28T14:04:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900250#M135872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wonder why you think that byte-mode would be a requirement on QDP LPDDR4?&lt;/P&gt;&lt;P&gt;Generally all LPDDR4, including the QDP ones, are running 16 bit wide per channel as a standard. &lt;BR /&gt;Operating the LPDDR4 components in byte-mode is just an optional way that the LPDDR4 memories allow, but the i.MX8 does not support it anyhow!&lt;/P&gt;&lt;P&gt;Thus I think you mixed something up.... there is no byte-mode-requirement for the i.MX8. In contrary, byte mode can not be used with i.MX8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX8 supports maximum 2 Chip Selects (=ranks), 2 Channels, 2 CKE.&lt;/P&gt;&lt;P&gt;Note: There are seperate pins for each channel's Chip-Select and CKE --&amp;gt; CS0_a, CS0_b, CS1_a, CS1_b&amp;nbsp; and same for CKE. So some people might misunderstand this as 4 CS and 4 CKE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="screenshot.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91204i6A426C09EEAF76EB/image-size/large?v=v2&amp;amp;px=999" role="button" title="screenshot.jpg" alt="screenshot.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2019 12:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900250#M135872</guid>
      <dc:creator>twmemphis</dc:creator>
      <dc:date>2019-07-15T12:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900251#M135873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thorsten,&lt;/P&gt;&lt;P&gt;Thank you for the information, I will pass this on to our designer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 10:53:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900251#M135873</guid>
      <dc:creator>gap</dc:creator>
      <dc:date>2019-07-16T10:53:58Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900252#M135874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more thing:&lt;/P&gt;&lt;P&gt;From a cost-perspective, DDR3L and DDR4 components are a lot cheaper "per Gigabit of Memory" than LPDDR4. Given todays market prices, LPDDR4 is almost twice as expensive than DDR3L or DDR4 for the same amount of memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But DDR3L and DDR4 components are only available in a x8 or x16 configuration, requiring to use multiple components to fill the bus-width of a rank. If you use a 32 bit wide bus, you would need to connect four pieces of x8 or two pieces of x16 components to each rank (with LPDDR4 you could just have one chip and you're done!).&lt;/P&gt;&lt;P&gt;Note: The i.MX8 supports maximum two ranks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both DDR4 and LPDDR4 are technologies which are limited to the worlds largest DRAM manufacturers. These big manufacturers require customers taking hundreds of millions of parts from them to fill their fab. Surely 99% or maybe more of the output of DDR4 and LPDDR4 goes into PC's, laptops, smartphones and tablets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now think about the following:&lt;/P&gt;&lt;P&gt;In latest a year all these applications will have changed to DDR5 and LPDDR5. The demand for DDR4 and LPDDR4 then might drop to only 1% of industrial customers. What do you think will the biggest manufacturers do? Will they continue making DDR4 and LPDDR4 ? I have doubts!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the past, with all former memory technologies, smaller "fabless" DRAM makers jumped on the technology and produced compatible alternative parts. But the bad news is: This door is almost closed as the production of high-capacity DDR4 and LPDDR4 components requires production-technologies of 20nm or smaller, which cost BILLIONS of dollars. Only the largest memory-firms can afford that. Eventually the one or another fabless company will simply buy the parts from the big companies and marks them with their own part number, but once the large manufacturer goes EOL, the product from the smaller company will die as well, as it is the same chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might only see some lower-density DDR4 and LPDDR4 from other fabless manufacturers which offer longevity. I know that Intelligent Memory has designed some DDR4 and LPDDR4 "with on-chip ECC error-correction" (which increases system-availability and reliability a lot!), but I do not yet see any other companies with plans for such parts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While DDR3L technology sounds "outdated" to some people, it will be the technology that can securely survive long-term, simple because there are lots of manufacturers offering such parts and the demand for DDR3L does not depend on mass-market applications like computers, phones or tables.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Thorsten Wronski&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Memphis Electronic AG&lt;/P&gt;&lt;P&gt;We Know Memory&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.memphis.ag"&gt;www.memphis.ag&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2019 12:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900252#M135874</guid>
      <dc:creator>twmemphis</dc:creator>
      <dc:date>2019-07-19T12:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900253#M135875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Thorsten,&lt;/P&gt;&lt;P&gt;Very interesting information, it has given us a lot to think about.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jul 2019 08:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/900253#M135875</guid>
      <dc:creator>gap</dc:creator>
      <dc:date>2019-07-28T08:12:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1206794#M167272</link>
      <description>&lt;P&gt;Hi Graeme,&lt;/P&gt;&lt;P&gt;Please send datasheet of&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;MT53D1024M32D4DT-053. I need to integrate it with imx8m quad processor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 10:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1206794#M167272</guid>
      <dc:creator>mathane89</dc:creator>
      <dc:date>2021-01-05T10:20:32Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1243880#M170674</link>
      <description>&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently working on imx8mm with 4GB as well. How did you get 4GB works? what changes you made ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the latest kernel and uboot version, and I enabled&amp;nbsp;CONFIG_IMX8M_4G_LPDDR4 in uboot and changed&amp;nbsp;#define PHYS_SDRAM_SIZE to 0xC0000000 to make it work on 3GB. But if I change to 4GB, it won't boot up and shows "Error found for upper 32 bits".&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea for that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jacob&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 05:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1243880#M170674</guid>
      <dc:creator>Jacob_bai</dc:creator>
      <dc:date>2021-03-11T05:48:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1361899#M182168</link>
      <description>&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;What changes have you made to support the&amp;nbsp;&lt;SPAN&gt;Micron MT53D1024M32D4DT-053 on our i.MX8M please let me know. I am trying to integrate the exact same part in out custom board design.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 20:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1361899#M182168</guid>
      <dc:creator>pratikfarkase</dc:creator>
      <dc:date>2021-10-26T20:17:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M-Mini 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1361900#M182169</link>
      <description>&lt;P&gt;Hi Felix,&lt;/P&gt;&lt;P&gt;What changes have you made to support the&amp;nbsp;&lt;SPAN&gt;Micron MT53D1024M32D4DT-053 on our i.MX8M please let me know. I am trying to integrate the exact same part in out custom board design.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 20:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-4GB-LPDDR4-RAM/m-p/1361900#M182169</guid>
      <dc:creator>pratikfarkase</dc:creator>
      <dc:date>2021-10-26T20:18:49Z</dc:date>
    </item>
  </channel>
</rss>