<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USB camera not detecting on IMX53-Start-R board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-camera-not-detecting-on-IMX53-Start-R-board/m-p/215702#M13586</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Siva,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB hardware is completely on-chip so I don't expect it to be a hardware issue.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I suspect the difference may be in the Linux kernel configuration or driver support or udev configuration.&lt;/P&gt;&lt;P&gt;I'm not a Linux engineer though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you see any messages reporting the connection of a USB device? If you do, then the camera is recognized at the USB level, but it may not have a driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Oct 2012 07:33:31 GMT</pubDate>
    <dc:creator>richard_stulens</dc:creator>
    <dc:date>2012-10-17T07:33:31Z</dc:date>
    <item>
      <title>USB camera not detecting on IMX53-Start-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-camera-not-detecting-on-IMX53-Start-R-board/m-p/215700#M13584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i insert the USB camera on IMX53-Start-R Board i am unable to detect the USB camera devices, But it's detecting the USB keypad and USB mouse.&lt;/P&gt;&lt;P&gt;Is there any configuration for USB camera detection on IMX53-Start-R board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to detecting the USB camera on IMX53-QSB board.&lt;/P&gt;&lt;P&gt;I want to know the difference between the IMX53-START-R board and IMX53-QSB&amp;nbsp; regarding USB detection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help us me to debug this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Ch.Siva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Oct 2012 13:39:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-camera-not-detecting-on-IMX53-Start-R-board/m-p/215700#M13584</guid>
      <dc:creator>chintakanisiva</dc:creator>
      <dc:date>2012-10-11T13:39:50Z</dc:date>
    </item>
    <item>
      <title>Re: USB camera not detecting on IMX53-Start-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-camera-not-detecting-on-IMX53-Start-R-board/m-p/215701#M13585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Siva Kumar!&lt;/P&gt;&lt;P&gt;Have you this problem on PC? Also, if you plan use this USB-camera for capture video it should be &lt;A href="http://www.ideasonboard.org/uvc/#status"&gt;http://www.ideasonboard.org/uvc/#status&lt;/A&gt;&lt;A href="http://www.ideasonboard.org/uvc/#status" title="http://www.ideasonboard.org/uvc/#status"&gt;&lt;BR /&gt;&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Oct 2012 09:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-camera-not-detecting-on-IMX53-Start-R-board/m-p/215701#M13585</guid>
      <dc:creator>BrilliantovKiri</dc:creator>
      <dc:date>2012-10-15T09:59:28Z</dc:date>
    </item>
    <item>
      <title>Re: USB camera not detecting on IMX53-Start-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-camera-not-detecting-on-IMX53-Start-R-board/m-p/215702#M13586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Siva,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB hardware is completely on-chip so I don't expect it to be a hardware issue.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I suspect the difference may be in the Linux kernel configuration or driver support or udev configuration.&lt;/P&gt;&lt;P&gt;I'm not a Linux engineer though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you see any messages reporting the connection of a USB device? If you do, then the camera is recognized at the USB level, but it may not have a driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2012 07:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-camera-not-detecting-on-IMX53-Start-R-board/m-p/215702#M13586</guid>
      <dc:creator>richard_stulens</dc:creator>
      <dc:date>2012-10-17T07:33:31Z</dc:date>
    </item>
  </channel>
</rss>