<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DDR Configuration Question</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899610#M135746</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i.MX6 MMDC supports 16-bit,&amp;nbsp;32-bit and&amp;nbsp;64-bit data bus, assuming &lt;/P&gt;&lt;P&gt;DRAM_D0 - DRAM_D15 as 16-bit bus, &lt;/P&gt;&lt;P&gt;DRAM_D0 - DRAM_D31 as 32-bit bus,&lt;/P&gt;&lt;P&gt;DRAM_D0 - DRAM_D63 as 64-bit bus.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Apr 2019 04:17:29 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2019-04-18T04:17:29Z</dc:date>
    <item>
      <title>DDR Configuration Question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899609#M135745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have designed a custom board based around the IMX6Q Sabre. A lot of the design is very similar, however we have gone for two 1GB RAM chips.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have used DDR3 channels 0 and 3. when we try to calibrate the RAM using the stress tester it sees we have 2x1GB but fails as it tries to calibrate channels 1 and 2. If we only calibrate channel 0 it passes with no problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is using channels 0 and 3 a valid configuration for the DDR or would I have to use channel 0 and 1?&lt;/P&gt;&lt;P&gt;If it is valid, how do I force the stress tester to ignore channels 1 and 2 during calibration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kyle.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 13:42:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899609#M135745</guid>
      <dc:creator>kcassar</dc:creator>
      <dc:date>2019-04-17T13:42:08Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Configuration Question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899610#M135746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i.MX6 MMDC supports 16-bit,&amp;nbsp;32-bit and&amp;nbsp;64-bit data bus, assuming &lt;/P&gt;&lt;P&gt;DRAM_D0 - DRAM_D15 as 16-bit bus, &lt;/P&gt;&lt;P&gt;DRAM_D0 - DRAM_D31 as 32-bit bus,&lt;/P&gt;&lt;P&gt;DRAM_D0 - DRAM_D63 as 64-bit bus.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 04:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899610#M135746</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-04-18T04:17:29Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Configuration Question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899611#M135747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for getting back to me.&lt;/P&gt;&lt;P&gt;Can it support 32 bit but using DRAM_D0 - DRAM_D15 and DRAM_D48 - DRAM_D63 and not using the middle 2 lanes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Kyle.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 08:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899611#M135747</guid>
      <dc:creator>kcassar</dc:creator>
      <dc:date>2019-04-18T08:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Configuration Question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899612#M135748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, the MMDC does not support&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;32 bit, using DRAM_D0 - DRAM_D15 and DRAM_D48 - DRAM_D63.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;~Yuri.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 10:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Configuration-Question/m-p/899612#M135748</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-04-18T10:26:14Z</dc:date>
    </item>
  </channel>
</rss>