<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx7ulp evk cannot enter download mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899375#M135703</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andre,&lt;/P&gt;&lt;P&gt;The DIP switch configuration that you mentioned are actually correct for Serial Downloader Mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80069iB52FA871919AF02B/image-size/large?v=v2&amp;amp;px=999" title="7ulp.png" alt="7ulp.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The other thing that you need to verify is that you are connecting the board to the PC trough the USB Type-C port (the one from the processor) instead of the micro USB (which is from USB-Serial converter).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 May 2019 20:25:35 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2019-05-02T20:25:35Z</dc:date>
    <item>
      <title>imx7ulp evk cannot enter download mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899374#M135702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't seem to figure out what I am doing wrong here. I have changed the boot-pins to download mode (D1 off, D2 on) but I can't detect anything on my PC.&lt;/P&gt;&lt;P&gt;If I use the SD card provided with the EVK then the linux distro boots fine (when i change back to dual boot settings (on, off, off, on).&lt;/P&gt;&lt;P&gt;Is there something I am missing here? With the imx7d sabre board I had to remove the SD card and then try to boot the system before the serial downloader worked, is there something similar that needs doing here?&lt;BR /&gt;I am attempting to load the android demo image from NXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2019 02:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899374#M135702</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2019-05-02T02:55:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx7ulp evk cannot enter download mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899375#M135703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andre,&lt;/P&gt;&lt;P&gt;The DIP switch configuration that you mentioned are actually correct for Serial Downloader Mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80069iB52FA871919AF02B/image-size/large?v=v2&amp;amp;px=999" title="7ulp.png" alt="7ulp.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The other thing that you need to verify is that you are connecting the board to the PC trough the USB Type-C port (the one from the processor) instead of the micro USB (which is from USB-Serial converter).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2019 20:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899375#M135703</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-05-02T20:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: imx7ulp evk cannot enter download mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899376#M135704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks - silly me, I think I didn't have the cable plugged in correctly...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was asking another question about the MIPI display but have now seen the hardware note that says that 5 resistors need to be removed and 5 0-ohm links need to be added, will do so after lunch.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 May 2019 00:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899376#M135704</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2019-05-03T00:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx7ulp evk cannot enter download mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899377#M135705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have also faced the same issue on my system and I directly reported this on &lt;A href="http://www. https//errorcode0x.com/fix-epson-error-code-0xf4/"&gt;epson error code 0xf4&lt;/A&gt;&amp;nbsp;and it is really very helpful to guide in this matter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 May 2019 06:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-evk-cannot-enter-download-mode/m-p/899377#M135705</guid>
      <dc:creator>watssonmerry445</dc:creator>
      <dc:date>2019-05-03T06:19:10Z</dc:date>
    </item>
  </channel>
</rss>