<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: uboot kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uboot-kernel/m-p/896747#M135469</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which board and which version of BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 May 2019 10:39:36 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2019-05-16T10:39:36Z</dc:date>
    <item>
      <title>uboot kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-kernel/m-p/896746#M135468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how can we update kernel image?we think as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1、there are two zImage patitions on emmc,one is old version and another is new version.&lt;/P&gt;&lt;P&gt;2、download the new kernel version and save in a partion,then uboot guide one of the two zImage to start&lt;/P&gt;&lt;P&gt;3、if succeed,update succeed,else the uboot will guide another zImage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 10:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-kernel/m-p/896746#M135468</guid>
      <dc:creator>youyong</dc:creator>
      <dc:date>2019-05-16T10:24:19Z</dc:date>
    </item>
    <item>
      <title>Re: uboot kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-kernel/m-p/896747#M135469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which board and which version of BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 10:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-kernel/m-p/896747#M135469</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-05-16T10:39:36Z</dc:date>
    </item>
    <item>
      <title>Re: uboot kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-kernel/m-p/896748#M135470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use the &lt;SPAN class=""&gt;TFTP&lt;/SPAN&gt; to update the zImage and file system.&lt;/P&gt;&lt;P&gt;FTP service will be used to transfer the kernel image from host to target every time the system reboots.&lt;/P&gt;&lt;P&gt;You can refer to&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1335"&gt;All Boards TFTP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-103717"&gt;https://community.nxp.com/docs/DOC-103717&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 10:51:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-kernel/m-p/896748#M135470</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-05-16T10:51:28Z</dc:date>
    </item>
  </channel>
</rss>