<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX6UL redundant interrupts</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-redundant-interrupts/m-p/896456#M135455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I develop driver for Linux which&amp;nbsp;need to count level changes on the line.&lt;/P&gt;&lt;P&gt;I register&amp;nbsp;my ISR at falling trigger, but I see hadler called on rising level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached some debug info as screenshots and minimal code I can reproduce the problem with.&lt;BR /&gt;&lt;BR /&gt;Why is ISR called redundantly? Would appreciate any thoughts on this.&lt;BR /&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Apr 2019 09:03:40 GMT</pubDate>
    <dc:creator>ilya_kondrashki</dc:creator>
    <dc:date>2019-04-30T09:03:40Z</dc:date>
    <item>
      <title>IMX6UL redundant interrupts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-redundant-interrupts/m-p/896456#M135455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I develop driver for Linux which&amp;nbsp;need to count level changes on the line.&lt;/P&gt;&lt;P&gt;I register&amp;nbsp;my ISR at falling trigger, but I see hadler called on rising level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached some debug info as screenshots and minimal code I can reproduce the problem with.&lt;BR /&gt;&lt;BR /&gt;Why is ISR called redundantly? Would appreciate any thoughts on this.&lt;BR /&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Apr 2019 09:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-redundant-interrupts/m-p/896456#M135455</guid>
      <dc:creator>ilya_kondrashki</dc:creator>
      <dc:date>2019-04-30T09:03:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL redundant interrupts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-redundant-interrupts/m-p/896457#M135456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ilya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what bsp used in the case, one can try with nxp linux from&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and try to debug it using sect.2.1.2 Interrupts (Operation) attached Linux Manual&lt;/P&gt;&lt;P&gt;AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4553.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4553.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Apr 2019 23:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-redundant-interrupts/m-p/896457#M135456</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-04-30T23:06:46Z</dc:date>
    </item>
  </channel>
</rss>