<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Disable i.MX6 UART from user application? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Disable-i-MX6-UART-from-user-application/m-p/896132#M135422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris,&lt;/P&gt;&lt;P&gt;From user applications, UART could be used as resources that could be locked or released. If you want to enable/disable them, and/or force logical levels on pins, you should use kernel operations and/or modified drivers to implement these functionalities.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 May 2019 23:00:58 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2019-05-16T23:00:58Z</dc:date>
    <item>
      <title>Disable i.MX6 UART from user application?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disable-i-MX6-UART-from-user-application/m-p/896131#M135421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to force both TX and RX pins of a UART to zero volts while I cycle the power of an attached peripheral. Is it possible to do this from a user application?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 13:42:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disable-i-MX6-UART-from-user-application/m-p/896131#M135421</guid>
      <dc:creator>chris_f</dc:creator>
      <dc:date>2019-05-15T13:42:35Z</dc:date>
    </item>
    <item>
      <title>Re: Disable i.MX6 UART from user application?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disable-i-MX6-UART-from-user-application/m-p/896132#M135422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris,&lt;/P&gt;&lt;P&gt;From user applications, UART could be used as resources that could be locked or released. If you want to enable/disable them, and/or force logical levels on pins, you should use kernel operations and/or modified drivers to implement these functionalities.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 23:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disable-i-MX6-UART-from-user-application/m-p/896132#M135422</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-05-16T23:00:58Z</dc:date>
    </item>
  </channel>
</rss>