<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 WiFi module integration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-module-integration/m-p/895513#M135335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I cannot make the Toradex Colibri iMX6ULL Wifi Module work using fsl repo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the image is running, there is not even any wireless interface detected when I try "ip a" or "ifconfig"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To begin with, how can I make the Wireless interface visible to the OS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From Toradex repo I could learn that the wifi used is mwifiex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Carrier board i'm using is: Aster V1.1B&lt;/P&gt;&lt;P&gt;The uP board is: Colibri imx6ull 512MB w/ WIFI (product id 0040....)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 May 2019 21:00:50 GMT</pubDate>
    <dc:creator>gbassi1</dc:creator>
    <dc:date>2019-05-15T21:00:50Z</dc:date>
    <item>
      <title>WiFi module integration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-module-integration/m-p/895513#M135335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I cannot make the Toradex Colibri iMX6ULL Wifi Module work using fsl repo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the image is running, there is not even any wireless interface detected when I try "ip a" or "ifconfig"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To begin with, how can I make the Wireless interface visible to the OS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From Toradex repo I could learn that the wifi used is mwifiex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Carrier board i'm using is: Aster V1.1B&lt;/P&gt;&lt;P&gt;The uP board is: Colibri imx6ull 512MB w/ WIFI (product id 0040....)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 21:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-module-integration/m-p/895513#M135335</guid>
      <dc:creator>gbassi1</dc:creator>
      <dc:date>2019-05-15T21:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi module integration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-module-integration/m-p/895514#M135336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gaston&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at toradex wifi solutions:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.toradex.com/knowledge-base/wifi" title="https://developer.toradex.com/knowledge-base/wifi"&gt;Wi-Fi&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 04:47:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-module-integration/m-p/895514#M135336</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-16T04:47:16Z</dc:date>
    </item>
  </channel>
</rss>