<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel booting bring up problem with imx6qpsdbre &amp; imx6dl custom board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-booting-bring-up-problem-with-imx6qpsdbre-imx6dl-custom/m-p/894698#M135226</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have some problem with between imx6qpsabresd-EV board and imx6dl-custom board.&lt;/P&gt;&lt;P&gt;I tested with&amp;nbsp;im6qpsabresd EV board, but designed custom board with imx6dl AP.&lt;/P&gt;&lt;P&gt;Here's my situation:&lt;/P&gt;&lt;P&gt;My custom board booting up only u-boot, Kernel booting stops at "Starting kernel"..., but when I put zImage in&amp;nbsp;&lt;SPAN&gt;mx6qpsabresd-EV board,&amp;nbsp;it works&amp;nbsp;fine booting up kernel. I don't understand this part because all kernel build environment is same between&amp;nbsp;imx6qp and&amp;nbsp;imx6dl.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm using same build environment as according to i.MX6 BSP manual. It says mx6qp and mx6dl build environment is same like as below&lt;/P&gt;&lt;P&gt;------------------------------------------below---------------------------&lt;/P&gt;&lt;P&gt;source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi&lt;BR /&gt;export ARCH=arm&lt;/P&gt;&lt;P&gt;make clean&lt;BR /&gt;make imx_v7_defconfig&lt;BR /&gt;make&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional information.&lt;/P&gt;&lt;P&gt;My custom board has different RAM size, so I used RAM stress tester and it passed everything. After that I put all revised RAM address&amp;nbsp;with&amp;nbsp;mxsabresd.cfg files and plug.s files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please share any information with this problem!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 May 2019 08:33:06 GMT</pubDate>
    <dc:creator>kwyang</dc:creator>
    <dc:date>2019-05-15T08:33:06Z</dc:date>
    <item>
      <title>Kernel booting bring up problem with imx6qpsdbre &amp; imx6dl custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-booting-bring-up-problem-with-imx6qpsdbre-imx6dl-custom/m-p/894698#M135226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have some problem with between imx6qpsabresd-EV board and imx6dl-custom board.&lt;/P&gt;&lt;P&gt;I tested with&amp;nbsp;im6qpsabresd EV board, but designed custom board with imx6dl AP.&lt;/P&gt;&lt;P&gt;Here's my situation:&lt;/P&gt;&lt;P&gt;My custom board booting up only u-boot, Kernel booting stops at "Starting kernel"..., but when I put zImage in&amp;nbsp;&lt;SPAN&gt;mx6qpsabresd-EV board,&amp;nbsp;it works&amp;nbsp;fine booting up kernel. I don't understand this part because all kernel build environment is same between&amp;nbsp;imx6qp and&amp;nbsp;imx6dl.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm using same build environment as according to i.MX6 BSP manual. It says mx6qp and mx6dl build environment is same like as below&lt;/P&gt;&lt;P&gt;------------------------------------------below---------------------------&lt;/P&gt;&lt;P&gt;source /opt/fsl-imx-fb/4.9.88-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi&lt;BR /&gt;export ARCH=arm&lt;/P&gt;&lt;P&gt;make clean&lt;BR /&gt;make imx_v7_defconfig&lt;BR /&gt;make&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional information.&lt;/P&gt;&lt;P&gt;My custom board has different RAM size, so I used RAM stress tester and it passed everything. After that I put all revised RAM address&amp;nbsp;with&amp;nbsp;mxsabresd.cfg files and plug.s files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please share any information with this problem!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 08:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-booting-bring-up-problem-with-imx6qpsdbre-imx6dl-custom/m-p/894698#M135226</guid>
      <dc:creator>kwyang</dc:creator>
      <dc:date>2019-05-15T08:33:06Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel booting bring up problem with imx6qpsdbre &amp; imx6dl custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-booting-bring-up-problem-with-imx6qpsdbre-imx6dl-custom/m-p/894699#M135227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kiwon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for different ddr size it is necessary to rebuild uboot with appropriate parameter&lt;/P&gt;&lt;P&gt;#define PHYS_SDRAM_SIZE in&amp;nbsp;uboot/include/configs/mx6sabresd.h &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6sabresd.h?h=imx_v2017.03_4.9.88_2.0.0_ga" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6sabresd.h?h=imx_v2017.03_4.9.88_2.0.0_ga"&gt;mx6sabresd.h\configs\include - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and fully rebuild image for custom "imx6dlsabresd" board&lt;/P&gt;&lt;P&gt;using sect.5.1 Build configurations attached Yocto Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 23:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-booting-bring-up-problem-with-imx6qpsdbre-imx6dl-custom/m-p/894699#M135227</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-15T23:42:09Z</dc:date>
    </item>
  </channel>
</rss>