<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: More than one LTIB on same hosts?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215178#M13521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using chroot to isolate BSP builds between an i.MX53 and i.MX6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Aug 2012 04:07:27 GMT</pubDate>
    <dc:creator>JimMalone</dc:creator>
    <dc:date>2012-08-29T04:07:27Z</dc:date>
    <item>
      <title>More than one LTIB on same hosts?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215173#M13516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Noob question.......&lt;/P&gt;&lt;P&gt;I have a mx53QSB and a mx28EVK and I have built systems in the past for both. I currently have the LTIB from my mx53QSB loaded and it is working great.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I now need to build for my mx28EVK, and can I use the same LTIB, or do I load both on the same machine?&lt;/P&gt;&lt;P&gt;Will this break something in the /opt/freescale directories? I am worried that they are at different versions and it might mess up the gcc build tree.&lt;/P&gt;&lt;P&gt;Am I off base or can it be done?&lt;/P&gt;&lt;P&gt;Can I pull LTIB from a git source that has both in them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would load the LTIB's as follows&lt;/P&gt;&lt;P&gt;MX53 in ~/mx53/ltib&lt;/P&gt;&lt;P&gt;MX28 in ~/mx28/ltib&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2012 00:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215173#M13516</guid>
      <dc:creator>JamesRobinson</dc:creator>
      <dc:date>2012-02-28T00:54:33Z</dc:date>
    </item>
    <item>
      <title>Re: More than one LTIB on same hosts?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215174#M13517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;I think I answered my own question. On the MX53QSB LTIB, I did a ./ltib -m selectype and took the mx28 option. I am in the middle of a build, so we shall see. The nice think is that if this works, I don't have to copy my .spec changes to the other build tree.&lt;/P&gt;&lt;P&gt;If anyone knows why I shouldn't do this, please let me know.&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2012 01:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215174#M13517</guid>
      <dc:creator>JamesRobinson</dc:creator>
      <dc:date>2012-02-28T01:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: More than one LTIB on same hosts?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215175#M13518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;James,&lt;/P&gt;&lt;P&gt;It's best to create a separate instance. &amp;nbsp;The SDKs for iMX53 may not be fully tested with the SDK you download for the iMX28. &amp;nbsp;Best to be safe.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2012 19:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215175#M13518</guid>
      <dc:creator>bonzo</dc:creator>
      <dc:date>2012-02-28T19:02:41Z</dc:date>
    </item>
    <item>
      <title>Re: More than one LTIB on same hosts?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215176#M13519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;James,&lt;/P&gt;&lt;P&gt;To extend upon what brad said I thought I would share how I've been&amp;nbsp;running many&amp;nbsp;BSP's side-by-side so it's easy to switch back and forth for various reasons.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here's an example of where I install various versions of LTIB in&amp;nbsp;my folder structure on my development machine - each version has an 'ltib' folder that's created during the installation process and a manually created 'pkgs' folder:&lt;/P&gt;&lt;P&gt;/opt/freescale/bsp/L2.6.35_10.08.01&lt;/P&gt;&lt;P&gt;/opt/freescale/bsp/L2.6.35_10.12.01&lt;/P&gt;&lt;P&gt;/opt/freescale/bsp/L2.6.35_11.04.01&lt;/P&gt;&lt;P&gt;/opt/freescale/bsp/L2.6.35_11.05.01&lt;/P&gt;&lt;P&gt;/opt/freescale/bsp/L2.6.35_11.09.01_MX50&lt;/P&gt;&lt;P&gt;/opt/freescale/bsp/L2.6.35_11.09.01_MX53&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in the /opt/freescale folder I store a handfull of simple shell scripts to switch back and forth using symbolic links:&lt;/P&gt;&lt;P&gt;setlinks_imx28_evk_10.08.sh&lt;/P&gt;&lt;P&gt;setlinks_imx28_evk_10.12.sh&lt;/P&gt;&lt;P&gt;setlinks_imx53_qsb_11.05.sh&lt;/P&gt;&lt;P&gt;setlinks_imx53_qsb_11.09.sh&lt;/P&gt;&lt;P&gt;setlinks_imx50_evk_11.04.sh&lt;/P&gt;&lt;P&gt;setlinks_imx50_evk_11.09.sh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sample shell script (setlinks_imx53_qsb_11.09.sh):&lt;/P&gt;&lt;P&gt;#!/bin/bash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;rm -f pkgs&lt;/P&gt;&lt;P&gt;rm -f ltib&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ln -s /opt/freescale/bsp/L2.6.35_11.09.01_MX53/ltib ltib&lt;/P&gt;&lt;P&gt;ln -s /opt/freescale/bsp/L2.6.35_11.09.01_MX53/pkgs pkgs&lt;/P&gt;&lt;P&gt;#end script&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This allows me to consistently use the /opt/freescale/ltib&amp;nbsp;and /opt/freescale/pkgs directories no matter which BSP I'm using to avoid my own confusion.&amp;nbsp; I can also have multiple copies of a BSP configured for&amp;nbsp;different target&amp;nbsp;boards&amp;nbsp;and be able to leave the configuration in-tact to rebuild the same version of BSP for a new board to work (this is nice when you're pulling in outside patches from the open source community).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using /opt/freescale and not&amp;nbsp;a custom installation folder was at one point recommended because of issues with customer install directories but may not be required anymore.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Switching between versions is as easy as running one of the shell scripts you reconfigure the symlinks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Feb 2012 20:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215176#M13519</guid>
      <dc:creator>JasonMoss</dc:creator>
      <dc:date>2012-02-29T20:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: More than one LTIB on same hosts?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215177#M13520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Even if you have all the packages in same folder, the conf spec will pick the right packages and versions from available pool.&lt;/P&gt;&lt;P&gt;So you dont have to worry about more.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2012 06:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215177#M13520</guid>
      <dc:creator>KrishnaPavan</dc:creator>
      <dc:date>2012-03-01T06:36:51Z</dc:date>
    </item>
    <item>
      <title>Re: More than one LTIB on same hosts?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215178#M13521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using chroot to isolate BSP builds between an i.MX53 and i.MX6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2012 04:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-one-LTIB-on-same-hosts/m-p/215178#M13521</guid>
      <dc:creator>JimMalone</dc:creator>
      <dc:date>2012-08-29T04:07:27Z</dc:date>
    </item>
  </channel>
</rss>