<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6Q -PCIE+i210 ethernet controller in u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893425#M135062</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Terry&lt;/P&gt;&lt;P&gt;for the i210 in defconfig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_NET_VENDOR_INTEL=y&lt;/P&gt;&lt;P&gt;CONFIG_IGB=y&lt;BR /&gt;CONFIG_IGB_HWMON=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;lspci&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;04:00.0 Ethernet controller: Intel Corporation I210 Gigabit Network Connection (rev 03)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also fighting the iMX6q with i210 and XR17V358 - The PCIe works on some PCBs work and not on other PCBs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Sep 2019 14:12:04 GMT</pubDate>
    <dc:creator>mike</dc:creator>
    <dc:date>2019-09-12T14:12:04Z</dc:date>
    <item>
      <title>IMX6Q -PCIE+i210 ethernet controller in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893420#M135057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have accustom hardware uses IMX6q which has a intel i210 ethernet controller connected to PCIE of IMX6Q , I had configured the PCIE in Kernel and enabled the e1000 driver , I am able to enumerate the controller ping works fine, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;whereas when I try to configure the controller and PCIE in UBoot, I see PCI driver listing the devices but the ethernet controller is not seen in the "NET:" looks like the e1000 driver is not getting linked to built-in.o&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help me with the correct configuration of the uboot for PCIE and e1000. (I am not using driver model, I am configuring my 2017 in the legacy way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Below is my Uboot log&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2017.03 (May 14 2019 - 14:22:34 -0700)&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.5 996 MHz (running at 792 MHz)&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Automotive temperature grade (-40C to 125C) at 55C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: iMX6q Sbare-SD&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 2 GiB&lt;BR /&gt;spi setup&lt;BR /&gt;&amp;nbsp;i2C INIT :&lt;BR /&gt;PMIC:&amp;nbsp; PFUZE100 ID=0x10&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;PCI:&lt;BR /&gt;&amp;nbsp; 00:01.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - 16c3:abcd - Bridge device&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 01:00.0&amp;nbsp;&amp;nbsp;&amp;nbsp; - 8086:1533 - Network controller&lt;BR /&gt;No panel detected: default to Hannstar-XGA&lt;BR /&gt;Display: Hannstar-XGA (1024x768)&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;=&amp;gt; pci&lt;BR /&gt;Scanning PCI devices on bus 0&lt;BR /&gt;BusDevFun&amp;nbsp; VendorId&amp;nbsp;&amp;nbsp; DeviceId&amp;nbsp;&amp;nbsp; Device Class&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sub-Class&lt;BR /&gt;_____________________________________________________________&lt;BR /&gt;00.01.00&amp;nbsp;&amp;nbsp; 0x16c3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xabcd&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bridge device&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x04&lt;BR /&gt;Cannot read bus configuration: -1&lt;BR /&gt;=&amp;gt; pci 1&lt;BR /&gt;Scanning PCI devices on bus 1&lt;BR /&gt;BusDevFun&amp;nbsp; VendorId&amp;nbsp;&amp;nbsp; DeviceId&amp;nbsp;&amp;nbsp; Device Class&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sub-Class&lt;BR /&gt;_____________________________________________________________&lt;BR /&gt;01.00.00&amp;nbsp;&amp;nbsp; 0x8086&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1533&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Network controller&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;Cannot read bus configuration: -1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; pci header 1&lt;BR /&gt;&amp;nbsp; vendor ID =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x16c3&lt;BR /&gt;&amp;nbsp; device ID =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xabcd&lt;BR /&gt;&amp;nbsp; command register ID =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0007&lt;BR /&gt;&amp;nbsp; status register =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0010&lt;BR /&gt;&amp;nbsp; revision ID =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x01&lt;BR /&gt;&amp;nbsp; class code =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x06 (Bridge device)&lt;BR /&gt;&amp;nbsp; sub class code =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x04&lt;BR /&gt;&amp;nbsp; programming interface =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;&amp;nbsp; cache line =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x08&lt;BR /&gt;&amp;nbsp; latency time =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;&amp;nbsp; header type =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x01&lt;BR /&gt;&amp;nbsp; BIST =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;&amp;nbsp; base address 0 =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x01000000&lt;BR /&gt;&amp;nbsp; base address 1 =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000000&lt;BR /&gt;&amp;nbsp; primary bus number =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;&amp;nbsp; secondary bus number =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x01&lt;BR /&gt;&amp;nbsp; subordinate bus number =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x01&lt;BR /&gt;&amp;nbsp; secondary latency timer =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;&amp;nbsp; IO base =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;&amp;nbsp; IO limit =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00&lt;BR /&gt;&amp;nbsp; secondary status =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000&lt;BR /&gt;&amp;nbsp; memory base =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0120&lt;BR /&gt;&amp;nbsp; memory limit =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0120&lt;BR /&gt;&amp;nbsp; prefetch memory base =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1000&lt;BR /&gt;&amp;nbsp; prefetch memory limit =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000&lt;BR /&gt;&amp;nbsp; prefetch memory base upper =&amp;nbsp; 0x00000000&lt;BR /&gt;&amp;nbsp; prefetch memory limit upper = 0x00000000&lt;BR /&gt;&amp;nbsp; IO base upper 16 bits =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000&lt;BR /&gt;&amp;nbsp; IO limit upper 16 bits =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000&lt;BR /&gt;&amp;nbsp; expansion ROM base address =&amp;nbsp; 0x01100000&lt;BR /&gt;&amp;nbsp; interrupt line =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xff&lt;BR /&gt;&amp;nbsp; interrupt pin =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x01&lt;BR /&gt;&amp;nbsp; bridge control =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2019 21:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893420#M135057</guid>
      <dc:creator>agnel_terry</dc:creator>
      <dc:date>2019-05-14T21:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q -PCIE+i210 ethernet controller in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893421#M135058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Terry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check ifdef CONFIG_PCI in uboot/include/configs/mx6sabresd.h&lt;/P&gt;&lt;P&gt;and test several cards&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6sabresd.h?h=imx_v2017.03_4.9.88_2.0.0_ga" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx6sabresd.h?h=imx_v2017.03_4.9.88_2.0.0_ga"&gt;mx6sabresd.h\configs\include - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 05:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893421#M135058</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-15T05:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q -PCIE+i210 ethernet controller in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893422#M135059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the response, the problem is not on the PCI/PCIE layer, as mentioned I am able to see the device getting listed in the PCI:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PCI:&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp; 00:01.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - 16c3:abcd - Bridge device&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp; 01:00.0&amp;nbsp;&amp;nbsp;&amp;nbsp; - 8086:1533 - Network controller&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;whereas its not seen in the NET :, The net shows only the IMX6 FEC, I had added "CONFIG_E1000=y" for the ethernet controller driver, still I don't see the device getting listed under,NET.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 16:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893422#M135059</guid>
      <dc:creator>agnel_terry</dc:creator>
      <dc:date>2019-05-15T16:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q -PCIE+i210 ethernet controller in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893423#M135060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Terry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as this is not specific imx issue this may be posted on uboot mail list&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lists.denx.de/listinfo/u-boot" title="https://lists.denx.de/listinfo/u-boot"&gt;U-Boot Info Page&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 23:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893423#M135060</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-15T23:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q -PCIE+i210 ethernet controller in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893424#M135061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Igor, will post it in the u-boot info page&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 16:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893424#M135061</guid>
      <dc:creator>agnel_terry</dc:creator>
      <dc:date>2019-05-16T16:14:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q -PCIE+i210 ethernet controller in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893425#M135062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Terry&lt;/P&gt;&lt;P&gt;for the i210 in defconfig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_NET_VENDOR_INTEL=y&lt;/P&gt;&lt;P&gt;CONFIG_IGB=y&lt;BR /&gt;CONFIG_IGB_HWMON=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;lspci&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;04:00.0 Ethernet controller: Intel Corporation I210 Gigabit Network Connection (rev 03)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also fighting the iMX6q with i210 and XR17V358 - The PCIe works on some PCBs work and not on other PCBs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 14:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/893425#M135062</guid>
      <dc:creator>mike</dc:creator>
      <dc:date>2019-09-12T14:12:04Z</dc:date>
    </item>
    <item>
      <title>回复： IMX6Q -PCIE+i210 ethernet controller in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/1536959#M196315</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a big problem and need your help.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.youtube.com/shorts/3jO6BhMUrl8" target="_blank"&gt;(47) Intel i210 Plug in crash - YouTube&lt;/A&gt;&lt;/P&gt;&lt;P&gt;My Board : Imx8mm&lt;/P&gt;&lt;P&gt;Linux version : 5.10&lt;/P&gt;&lt;P&gt;Ethernet Card : Intel I210&lt;/P&gt;&lt;P&gt;When I plugged in the line to RJ45, this is the kernel messaage.&lt;/P&gt;&lt;P&gt;Please give me a hand.&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[ 1645.118487] igb 0000:01:00.0: Detected Tx Unit Hang 1011-1 XXXXXXXX&lt;BR /&gt;[ 1645.118487] Tx Queue &amp;lt;3&amp;gt;&lt;BR /&gt;[ 1645.118487] TDH &amp;lt;0&amp;gt;&lt;BR /&gt;[ 1645.118487] TDT &amp;lt;1&amp;gt;&lt;BR /&gt;[ 1645.118487] next_to_use &amp;lt;1&amp;gt;&lt;BR /&gt;[ 1645.118487] next_to_clean &amp;lt;0&amp;gt;&lt;BR /&gt;[ 1645.118487] buffer_info[next_to_clean]&lt;BR /&gt;[ 1645.118487] time_stamp &amp;lt;100051ed0&amp;gt;&lt;BR /&gt;[ 1645.118487] next_to_watch &amp;lt;0000000037bbc16b&amp;gt;&lt;BR /&gt;[ 1645.118487] jiffies &amp;lt;100052197&amp;gt;&lt;BR /&gt;[ 1645.118487] desc.status &amp;lt;4f4000&amp;gt;&lt;BR /&gt;[ 1647.839563] ------------[ cut here ]------------&lt;BR /&gt;[ 1647.844215] 1007-3 XXXX NETDEV WATCHDOG: eth1 (igb): transmit queue 0 timed out&lt;BR /&gt;[ 1647.851607] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:485 dev_watchdog+0x300/0x310&lt;BR /&gt;[ 1647.859876] Modules linked in: overlay fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine rng_core authenc libdes crct10dif_ce caam secvio error gpio_ir_recv rc_core fuse&lt;BR /&gt;[ 1647.877395] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 5.10.72-lts-5.10.y+g22ec7e8cbace #1&lt;BR /&gt;[ 1647.885570] Hardware name: FSL i.MX8MM EVK board (DT)&lt;BR /&gt;[ 1647.890624] pstate: 20000005 (nzCv daif -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 1647.896635] pc : dev_watchdog+0x300/0x310&lt;BR /&gt;[ 1647.900647] lr : dev_watchdog+0x300/0x310&lt;BR /&gt;[ 1647.904656] sp : ffff800011d4bd90&lt;BR /&gt;[ 1647.907970] x29: ffff800011d4bd90 x28: ffff0000c0e9f940&lt;BR /&gt;[ 1647.913287] x27: 0000000000000004 x26: ffff0000c180c480&lt;BR /&gt;[ 1647.918605] x25: 0000000000000140 x24: 00000000ffffffff&lt;BR /&gt;[ 1647.923923] x23: ffff0000c180c3dc x22: 0000000000000000&lt;BR /&gt;[ 1647.929238] x21: ffff800011b36000 x20: ffff0000c180c000&lt;BR /&gt;[ 1647.934554] x19: 0000000000000000 x18: 0000000000000030&lt;BR /&gt;[ 1647.939869] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 1647.945185] x15: ffff800011b427f8 x14: 4454454e20585858&lt;BR /&gt;[ 1647.950501] x13: ffff800011b517b0 x12: 00000000000005eb&lt;BR /&gt;[ 1647.955818] x11: 00000000000001f9 x10: ffff800011ba97b0&lt;BR /&gt;[ 1647.961136] x9 : 00000000fffff000 x8 : ffff800011b517b0&lt;BR /&gt;[ 1647.966453] x7 : ffff800011ba97b0 x6 : 0000000000000003&lt;BR /&gt;[ 1647.971768] x5 : 0000000000000000 x4 : 0000000000000000&lt;BR /&gt;[ 1647.977084] x3 : 0000000000000000 x2 : 0000000000000100&lt;BR /&gt;[ 1647.982399] x1 : 298971a5ac26f600 x0 : 0000000000000000&lt;BR /&gt;[ 1647.987716] Call trace:&lt;BR /&gt;[ 1647.990166] dev_watchdog+0x300/0x310&lt;BR /&gt;[ 1647.993834] call_timer_fn.constprop.0+0x24/0x80&lt;BR /&gt;[ 1647.998454] __run_timers.part.0+0x1f4/0x22c&lt;BR /&gt;[ 1648.002726] run_timer_softirq+0x3c/0x7c&lt;BR /&gt;[ 1648.006651] efi_header_end+0x124/0x290&lt;BR /&gt;[ 1648.010490] irq_exit+0xdc/0xfc&lt;BR /&gt;[ 1648.013634] __handle_domain_irq+0x80/0xe0&lt;BR /&gt;[ 1648.017733] gic_handle_irq+0xc0/0x140&lt;BR /&gt;[ 1648.021483] el1_irq+0xcc/0x180&lt;BR /&gt;[ 1648.024629] cpuidle_enter_state+0x130/0x2f0&lt;BR /&gt;[ 1648.028901] cpuidle_enter+0x38/0x50&lt;BR /&gt;[ 1648.032480] do_idle+0x218/0x2a0&lt;BR /&gt;[ 1648.035710] cpu_startup_entry+0x24/0x70&lt;BR /&gt;[ 1648.039636] rest_init+0xd8/0xe8&lt;BR /&gt;[ 1648.042869] arch_call_rest_init+0x10/0x1c&lt;BR /&gt;[ 1648.046966] start_kernel+0x4ac/0x4e4&lt;BR /&gt;[ 1648.050629] ---[ end trace a9279d2e8a564f58 ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 08:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-PCIE-i210-ethernet-controller-in-u-boot/m-p/1536959#M196315</guid>
      <dc:creator>tzeng015</dc:creator>
      <dc:date>2022-10-13T08:19:39Z</dc:date>
    </item>
  </channel>
</rss>