<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8M and PCIe rescan in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892460#M134910</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to rescan my Pcie devices after booting but it doesn't work.&lt;/P&gt;&lt;P&gt;The command used for rescan is : "echo 1 &amp;gt; /sys/bus/pci/rescan"&lt;/P&gt;&lt;P&gt;This command is very very fast and gives no output. "Lspci" gives nothing. If i reboot my IMX8M card, i can see my pcie devices.&lt;/P&gt;&lt;P&gt;Have you got an idea about the problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(I use yocto with BSP and kernel 4.14.78)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frederic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Apr 2019 12:18:54 GMT</pubDate>
    <dc:creator>fredericduchass</dc:creator>
    <dc:date>2019-04-11T12:18:54Z</dc:date>
    <item>
      <title>IMX8M and PCIe rescan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892460#M134910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to rescan my Pcie devices after booting but it doesn't work.&lt;/P&gt;&lt;P&gt;The command used for rescan is : "echo 1 &amp;gt; /sys/bus/pci/rescan"&lt;/P&gt;&lt;P&gt;This command is very very fast and gives no output. "Lspci" gives nothing. If i reboot my IMX8M card, i can see my pcie devices.&lt;/P&gt;&lt;P&gt;Have you got an idea about the problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(I use yocto with BSP and kernel 4.14.78)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frederic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 12:18:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892460#M134910</guid>
      <dc:creator>fredericduchass</dc:creator>
      <dc:date>2019-04-11T12:18:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M and PCIe rescan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892461#M134911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As a workaround you can powercycle PCI with /sys/devices/platform/*.pcie/power/control entry.&lt;BR /&gt;Here "*" depends on the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2019 04:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892461#M134911</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-04-12T04:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M and PCIe rescan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892462#M134912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;PRE&gt;Hello Victor,

I read that : 

The /sys/devices/.../power/control attribute allows the user   space to control the run-time power management of the device.    All devices have one of the following two values for the   power/control file:    + "auto\n" to allow the device to be power managed at run time;   + "on\n" to prevent the device from being power managed;    The default for all devices is "auto", which means that they may   be subject to automatic power management, depending on their   drivers.  Changing this attribute to "on" prevents the driver   from power managing the device at run time.  Doing that while   the device is suspended causes it to be woken up.

How i can reboot the pcie link with control and only "on" or "auto" ?&lt;/PRE&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Frederic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2019 06:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892462#M134912</guid>
      <dc:creator>fredericduchass</dc:creator>
      <dc:date>2019-04-12T06:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M and PCIe rescan</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892463#M134913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to rescan with the commands like these:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;echo 1 &amp;gt; /sys/bus/pci/devices/0000\:00\:00.0/rescan&lt;BR /&gt;echo 1 &amp;gt; /sys/bus/pci/rescan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 09:12:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-and-PCIe-rescan/m-p/892463#M134913</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-05-16T09:12:09Z</dc:date>
    </item>
  </channel>
</rss>