<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックecspi1 write data slow</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ecspi1-write-data-slow/m-p/891343#M134744</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We connect one 240*320 SPI interface LCD to ecspi1 and developed it's driver on Yocto BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It can display UI now, but&amp;nbsp;flash frame rate is very slow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you suggest how to improve spi speed? thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here&amp;nbsp;is its DTS config&lt;/P&gt;&lt;P&gt;&amp;amp;ecspi1 {&lt;BR /&gt; compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";&lt;BR /&gt; fsl,spi-num-chipselects = &amp;lt;1&amp;gt;;&lt;BR /&gt; cs-gpios = &amp;lt;&amp;amp;gpio4 9 0&amp;gt;;&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ecspi1&amp;gt;;&lt;BR /&gt; status = "okay";&lt;BR /&gt; lcd:startek@0 {&lt;BR /&gt; compatible = "startek,startek-lcd";&lt;BR /&gt; #address-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt; #size-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ecspi1_rest&amp;gt;;&lt;BR /&gt; spi-max-frequency = &amp;lt;20000000&amp;gt;;&lt;BR /&gt; rest-gpios = &amp;lt;&amp;amp;gpio6 11 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt; rs-gpios = &amp;lt;&amp;amp;gpio4 8 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt; reg = &amp;lt;0&amp;gt;;&lt;BR /&gt; };&lt;BR /&gt;};&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Apr 2019 08:55:33 GMT</pubDate>
    <dc:creator>brli</dc:creator>
    <dc:date>2019-04-25T08:55:33Z</dc:date>
    <item>
      <title>ecspi1 write data slow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ecspi1-write-data-slow/m-p/891343#M134744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We connect one 240*320 SPI interface LCD to ecspi1 and developed it's driver on Yocto BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It can display UI now, but&amp;nbsp;flash frame rate is very slow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you suggest how to improve spi speed? thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here&amp;nbsp;is its DTS config&lt;/P&gt;&lt;P&gt;&amp;amp;ecspi1 {&lt;BR /&gt; compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";&lt;BR /&gt; fsl,spi-num-chipselects = &amp;lt;1&amp;gt;;&lt;BR /&gt; cs-gpios = &amp;lt;&amp;amp;gpio4 9 0&amp;gt;;&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ecspi1&amp;gt;;&lt;BR /&gt; status = "okay";&lt;BR /&gt; lcd:startek@0 {&lt;BR /&gt; compatible = "startek,startek-lcd";&lt;BR /&gt; #address-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt; #size-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ecspi1_rest&amp;gt;;&lt;BR /&gt; spi-max-frequency = &amp;lt;20000000&amp;gt;;&lt;BR /&gt; rest-gpios = &amp;lt;&amp;amp;gpio6 11 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt; rs-gpios = &amp;lt;&amp;amp;gpio4 8 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt; reg = &amp;lt;0&amp;gt;;&lt;BR /&gt; };&lt;BR /&gt;};&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Apr 2019 08:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ecspi1-write-data-slow/m-p/891343#M134744</guid>
      <dc:creator>brli</dc:creator>
      <dc:date>2019-04-25T08:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: ecspi1 write data slow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ecspi1-write-data-slow/m-p/891344#M134745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi br&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to use dma, as in ecspi5 example :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6q.dtsi?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6q.dtsi?h=imx_4.14.78_1.0.0_ga"&gt;imx6q.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also one can try to increase burst size using BURST_LENGTH register ECSPIx_CONREG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Apr 2019 23:31:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ecspi1-write-data-slow/m-p/891344#M134745</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-04-25T23:31:59Z</dc:date>
    </item>
  </channel>
</rss>