<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic question for /dev/fb0 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/question-for-dev-fb0/m-p/890503#M134653</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please tell that whether the func cfb_imageblit(...) in file cfbimgblt.c used for ?&lt;/P&gt;&lt;P&gt;I am porting lcdc on IMX7D,I just want to know if function&amp;nbsp; cfb_imageblit is needed when open /dev/fb0 to flush image in userspace test code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Apr 2019 08:40:35 GMT</pubDate>
    <dc:creator>guojunqiang</dc:creator>
    <dc:date>2019-04-24T08:40:35Z</dc:date>
    <item>
      <title>question for /dev/fb0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/question-for-dev-fb0/m-p/890503#M134653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please tell that whether the func cfb_imageblit(...) in file cfbimgblt.c used for ?&lt;/P&gt;&lt;P&gt;I am porting lcdc on IMX7D,I just want to know if function&amp;nbsp; cfb_imageblit is needed when open /dev/fb0 to flush image in userspace test code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 08:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/question-for-dev-fb0/m-p/890503#M134653</guid>
      <dc:creator>guojunqiang</dc:creator>
      <dc:date>2019-04-24T08:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: question for /dev/fb0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/question-for-dev-fb0/m-p/890504#M134654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi keil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what bsp used in the case and driver source. Just&lt;/P&gt;&lt;P&gt;for reference one can look at driver descriptions in attached Linux Manual&lt;/P&gt;&lt;P&gt;sect.6.3.4 ELCDIF Frame Buffer, sect.6.4.5 Electrophoretic Display Controller (EPDC) Interface&lt;/P&gt;&lt;P&gt;Linux L4.14.78_1.0.0&amp;nbsp;&amp;nbsp;&amp;nbsp; link&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga" target="test_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Apr 2019 01:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/question-for-dev-fb0/m-p/890504#M134654</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-04-25T01:00:17Z</dc:date>
    </item>
  </channel>
</rss>