<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6UL Using CAAM Memory More Than 16 KB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Using-CAAM-Memory-More-Than-16-KB/m-p/888011#M134405</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The device tree file states about i.MX6Q compatibility.&lt;/P&gt;&lt;P&gt;IMX6Q CAAM&amp;nbsp; has 16 KB secure RAM.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Apr 2019 06:10:21 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2019-04-11T06:10:21Z</dc:date>
    <item>
      <title>iMX6UL Using CAAM Memory More Than 16 KB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Using-CAAM-Memory-More-Than-16-KB/m-p/888010#M134404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently using an iMX6UL secure chip. According to the Reference Manual, CAAM starts at the address 0010_0000 and ends at the address 0010_7FFF. The total size is 32KB.&lt;/P&gt;&lt;P&gt;However, in the device tree include file "imx6ul.dtsi" following memory&amp;nbsp;size is allocated to the CAAM memory:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;caam_sm: caam-sm@00100000 {
compatible = "fsl,imx7d-caam-sm", "fsl,imx6q-caam-sm";
reg = &amp;lt;0x00100000 &lt;STRONG&gt;0x3fff&lt;/STRONG&gt;&amp;gt;;
};&lt;/PRE&gt;&lt;P&gt;As can be seen above, the amount of size allocated is 0x3fff, which is less than 16KB.&lt;/P&gt;&lt;P&gt;Any idea what could be the reason to define it like above?&lt;/P&gt;&lt;P&gt;I wanted to use further CAAM RAM more than 16KB, however, it fails when mapping virtual memory at the 5th Page.&lt;/P&gt;&lt;P&gt;Linux BSP version I am using: 3.14.38&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 08:18:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Using-CAAM-Memory-More-Than-16-KB/m-p/888010#M134404</guid>
      <dc:creator>radikedalpatadu</dc:creator>
      <dc:date>2019-04-09T08:18:21Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6UL Using CAAM Memory More Than 16 KB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Using-CAAM-Memory-More-Than-16-KB/m-p/888011#M134405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The device tree file states about i.MX6Q compatibility.&lt;/P&gt;&lt;P&gt;IMX6Q CAAM&amp;nbsp; has 16 KB secure RAM.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 06:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-Using-CAAM-Memory-More-Than-16-KB/m-p/888011#M134405</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-04-11T06:10:21Z</dc:date>
    </item>
  </channel>
</rss>