<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DDR Test in Initramfs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-in-Initramfs/m-p/885110#M134106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can load data into RAM and check the CRC with crc32 command. Here is an example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; fatload mmc 0:1 0x80800000 zImage&lt;BR /&gt;reading zImage&lt;BR /&gt;6616232 bytes read in 295 ms (21.4 MiB/s)&lt;BR /&gt;=&amp;gt; crc32 0x80800000 0x64F4A8&lt;BR /&gt;CRC32 for 80800000 ... 80e4f4a7 ==&amp;gt; a9ceef28&lt;BR /&gt;=&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Mar 2019 07:39:25 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-03-13T07:39:25Z</dc:date>
    <item>
      <title>DDR Test in Initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-in-Initramfs/m-p/885109#M134105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Initramfs loading in MFG tool. Validating DDR data lines and Address lines from Uboot.&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; DDR test is pass(Below prints are displayed in console).&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;DDR Test Pass &lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But when ddr testing is completed, Kernel is not loading , below is boot log for reference &lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x4a7ab0 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 83800000 ...&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; PRFYC Initramfs&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux RAMDisk Image (uncompressed)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 13550857 Bytes = 12.9 MiB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... Bad Data CRC&lt;BR /&gt;Ramdisk image is corrupt or invalid&lt;BR /&gt;G18M&amp;gt; &lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please&amp;nbsp; let me know, how to validate the ddr data line and address line in uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Haji&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 06:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-in-Initramfs/m-p/885109#M134105</guid>
      <dc:creator>hajimohammed</dc:creator>
      <dc:date>2019-03-12T06:37:09Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Test in Initramfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-in-Initramfs/m-p/885110#M134106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can load data into RAM and check the CRC with crc32 command. Here is an example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; fatload mmc 0:1 0x80800000 zImage&lt;BR /&gt;reading zImage&lt;BR /&gt;6616232 bytes read in 295 ms (21.4 MiB/s)&lt;BR /&gt;=&amp;gt; crc32 0x80800000 0x64F4A8&lt;BR /&gt;CRC32 for 80800000 ... 80e4f4a7 ==&amp;gt; a9ceef28&lt;BR /&gt;=&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Mar 2019 07:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-in-Initramfs/m-p/885110#M134106</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-03-13T07:39:25Z</dc:date>
    </item>
  </channel>
</rss>