<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PSWITCH on imx23 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PSWITCH-on-imx23/m-p/884432#M134016</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a student making a custom system on a PCB with the imx23 processor. I left my PSWITCH pin as no connect. But i read that it should be pulled to VDD in order for the system to boot up, did i read that right? i read the power-up part in the manual and it lists either a 5V power supply or PSWITCH pull to above 1 v for 100 ms. So do i need to connect PSWITCH to anything?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attach my .sch and .brd file, please comment, feeback for improvement greatly appreciated. The files are&amp;nbsp;attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;problem i faced so far:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. processor not booting up, 2.5v rail reads 5v,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is one way to check if processor boot correctly? attached a PC to the USB pins to see if there are any output? or put a serial console on the USB Debug pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Feb 2019 02:45:04 GMT</pubDate>
    <dc:creator>adoan28</dc:creator>
    <dc:date>2019-02-05T02:45:04Z</dc:date>
    <item>
      <title>PSWITCH on imx23</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PSWITCH-on-imx23/m-p/884432#M134016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a student making a custom system on a PCB with the imx23 processor. I left my PSWITCH pin as no connect. But i read that it should be pulled to VDD in order for the system to boot up, did i read that right? i read the power-up part in the manual and it lists either a 5V power supply or PSWITCH pull to above 1 v for 100 ms. So do i need to connect PSWITCH to anything?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attach my .sch and .brd file, please comment, feeback for improvement greatly appreciated. The files are&amp;nbsp;attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;problem i faced so far:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. processor not booting up, 2.5v rail reads 5v,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is one way to check if processor boot correctly? attached a PC to the USB pins to see if there are any output? or put a serial console on the USB Debug pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 02:45:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PSWITCH-on-imx23/m-p/884432#M134016</guid>
      <dc:creator>adoan28</dc:creator>
      <dc:date>2019-02-05T02:45:04Z</dc:date>
    </item>
    <item>
      <title>Re: PSWITCH on imx23</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PSWITCH-on-imx23/m-p/884433#M134017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PSWITCH is described in sect.32.4 PSWITCH Pin Functions Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/reference-manual/IMX23RM.pdf" title="https://www.nxp.com/docs/en/reference-manual/IMX23RM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/IMX23RM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for PSWITCH connections one can check&lt;/P&gt;&lt;P&gt;Schematics (2)&lt;BR /&gt;i.MX23 EVK Design Files for Rev C boards: Hardware Schematics, Gerbers, &lt;BR /&gt;OrCAD files and System BOM(REV 1.1)&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx23-evaluation-kit:IMX23EVK?tab=Design_Tools_Tab" title="https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx23-evaluation-kit:IMX23EVK?tab=Design_Tools_Tab"&gt;i.MX23 Evaluation Kit|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note, this processor is very old and not supported in nxp software, one can check&lt;/P&gt;&lt;P&gt;third party resources like&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.olimex.com/wiki/IMX233" title="https://www.olimex.com/wiki/IMX233"&gt;IMX233 - Olimex&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;usually wrong voltages are caused by brownouts, may be useful to check&lt;/P&gt;&lt;P&gt;(i.MX28 power system is similar to i.MX23)&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.digi.com/support/knowledge-base/brown-out-issues-on-connectcard-wi-i-mx28-modules" title="https://www.digi.com/support/knowledge-base/brown-out-issues-on-connectcard-wi-i-mx28-modules"&gt;Brown out issues on ConnectCard (Wi)i.mx28 modules | Digi International&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 23:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PSWITCH-on-imx23/m-p/884433#M134017</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-02-05T23:31:27Z</dc:date>
    </item>
  </channel>
</rss>