<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Is kobs-ng extract command correct?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883507#M133895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andreamarson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just as an update, since this is not an official NXP&amp;nbsp;release the best alternative would be adding a comment or opening an issue directly on the repository.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 May 2019 19:33:16 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-05-02T19:33:16Z</dc:date>
    <item>
      <title>Is kobs-ng extract command correct?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883505#M133893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I understand correctly the code, I think that the function &lt;SPAN class=""&gt;mtd_load_all_boot_structures is incorrect:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/NXPmicro/imx-kobs/blob/228dbb9b1a202892d884bd01985dd3522ad49d59/src/mtd.c#L1454" title="https://github.com/NXPmicro/imx-kobs/blob/228dbb9b1a202892d884bd01985dd3522ad49d59/src/mtd.c#L1454"&gt;imx-kobs/mtd.c at 228dbb9b1a202892d884bd01985dd3522ad49d59 · NXPmicro/imx-kobs · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It assumes that the NCB data structures are always used, no matter which SOC knobs-ng is running on.&lt;/P&gt;&lt;P&gt;I think this function should detect the SOC and behave accordingly instead, as the data structures used by the bootrom have changed over time.&lt;/P&gt;&lt;P&gt;Am I right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 10:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883505#M133893</guid>
      <dc:creator>andreamarson</dc:creator>
      <dc:date>2019-03-11T10:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: Is kobs-ng extract command correct?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883506#M133894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andreamarson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will check with the maintainers of this code. It’s true that it seems that the code does not check for the SOC in this step, probably assuming you will provide the right parameters.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 17:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883506#M133894</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-04-18T17:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: Is kobs-ng extract command correct?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883507#M133895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andreamarson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just as an update, since this is not an official NXP&amp;nbsp;release the best alternative would be adding a comment or opening an issue directly on the repository.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 May 2019 19:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883507#M133895</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-05-02T19:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: Is kobs-ng extract command correct?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883508#M133896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi gusarambula,&lt;BR /&gt;thank you for your feedback.&lt;/P&gt;&lt;P&gt;Does NXP provide an official version of kobs-ng supporting all the different versions of i.MX SOC/bootroms?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jun 2019 09:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-kobs-ng-extract-command-correct/m-p/883508#M133896</guid>
      <dc:creator>andreamarson</dc:creator>
      <dc:date>2019-06-03T09:52:48Z</dc:date>
    </item>
  </channel>
</rss>